Part Number: MSP430FR2673 Hi Team,
There's an issue from the customer need your help:
I tried to restart the 430 chip through WDT or configure reset register, and it did restart and begin running, but via simulation found that some of register not…
Part Number: MSP430FR2673 Hi Team,
There's an issue from the customer need your help:
I've placed two apps inside the 2673 chip, one as an upgrade boot and the other as an app, and the upgrade boot is written refer to BSL. When the newly upgraded…
Part Number: MSP430FR2673 Other Parts Discussed in Thread: MSP430FR2633 Hello,
My customer would like to know power consumption data for captivate on MSP430FR2673.
I found some data for MSP430FR2633 in captivate design guide. But I couldn't find for FR2673…
Part Number: MSP430FR2673
Hi team,
Here's an issue from the customer may need your help:
Firmware transfer issues were encountered while upgrading using the BSL that comes with the MSP430. The rx_password write is OK after the 430 slave enters the…
Part Number: MSP430FR2673 Other Parts Discussed in Thread: MSP-FET Hello,
I have some questions for BSL in MSP430FR2673.
My customer put a 10nF instead of 1nF on RST pin to improve noise performance. They don’t use both JTAG and Spy-bi-wire on their…
Part Number: MSP430FR2673 Hello,
The datasheet recommend to put a 10nF capacitor if JTAG/Spi-bi-Wire are not used. Is it possible to increase this capacitor value to improve noise tolerance?
Regards, Oba
Part Number: MSP430FR2673 Hi experts,
Q1:If the Automatic Power Down function is disabled (default), what kind of processing will be performed, and will there be a delay?
Automatic Power Down: software-dl.ti.com/.../Auto_Power_Down.html
Q2:Is it correct…
Part Number: MSP430FR2673 Hello,
Our customer is considering to use MSP430FR267x for a 4-20mA application. So the peak current consumption is important for them. Then they would like to know the current consumption during power-up. Do you have any data? …
Part Number: MSP430FR2673 Hello,
My customer has a question for unused IO pins.
The user’s guide recommend to leave unused IO pins unconnected and configure them as OUTPUT in user’s S/W.
Is that the best way for the lowest power consumption…