Other Parts Discussed in Thread: MSP430FR5849 Hello.
I want to measure input pulse duty using timer capture mode on MSP430FR5849.
Max Frequency will be 1MHz and pin assign is P1.2
When I tested the function, I could get a steady value to 500 KHz. However…
Great to hear. BTW, I got one of my MSP430FR5849 CC8 projects up and running with only a few hiccups (compiler couldn't find intrinsics.h, linker couldn't find liba.c) which, compared to my efforts to get an Xcode project moving was pretty painless.…
Sorry, the question should be revised. They want to compare it with pins and functionality of msp430fr5849 instead of MSP430F2254IDA .
Can you please help us know if Pins and functions of MSP430F5437A are compatible with those of msp430fr5849 instead of …
sir i tried this code for msp430fr5849 it is working ok but in my project my device is msp430f1611 and when i change this device it gives the error
TIMER_A0_BASE
Hi Ravi,
I slightly modified my SPI transmit and receive routines to allow for a variable number of bytes to be transmitted or received. Everything works fine now. writing left and right attenuation registers and reading the SRC ratio registers individually…
Part Number: MSP430FR5949 Other Parts Discussed in Thread: MSP430FR5849 , MSP-FET , Tool/software: Code Composer Studio Hi,
I have seen this issue popping up in several E2E threads but have difficulties finding an answer that works for me.
I am using own…
Other Parts Discussed in Thread: MSP430FR5849 I have just downloaded the latest version of CCS V6.1 and am having problem compiling my code.
I have a simple project and have used Grace to configure a MSP430FR5849 device.
However when I compile the code…
Other Parts Discussed in Thread: MSP-FET , MSP430F5659 , MSP430FR5849 , MSP430F5528 , MSP430F5310 , MSP430L092 , MSP430FR5969 I purchased the newer black MSP-FET tool and use with IAR tools. It is constantly asking to update the FET firmware and complains about…
I'm having the same issues with the MSP-FET while debugging an MSP430FR5849. I tried using a debugger with an older firmware by selecting "ignore" on the firmware update prompt, but the problem still remains.
I also have to disable and enable…
Other Parts Discussed in Thread: MSP430FR5849 I am trying to allocate a 4K array in FRAM used for data logging and have followed the procedure from "Creating MSP430 FRAM Variables Using CCS" post.
It appears to allocate the buffer but I am getting…