Part Number: MSP430FR5857 Tool/software: Code Composer Studio Hi,
I'm attempting to use the Qmath fuctions, however the library is not linking properly. I have tried moving "libmath.a" to the top of "--library,-l" in the File Search Path property of the…
Part Number: MSP430FR5857 Other Parts Discussed in Thread: MSPWARE Tool/software: Code Composer Studio /* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary…
Part Number: MSP430FR5857 Tool/software: Code Composer Studio I am designing a board with the above mentioned MCU. I am trying to program using an eZ-FET Lite.
The connections I made were
On ez-FET lite On my Board
3.3V ----------------> AVcc/DVcc …
Part Number: MSP430FR5857 Tool/software: Code Composer Studio My design needs a pin to be low for 5 minutes and then on for 5 secs and want to repeat endlessly. I thought of using the timer for this.
#include <msp430.h>
unsigned int i=1;
int main(void…
Part Number: MSP430FR5857 The PxSEL0 and PxSEL1 and used to select the function that the GPIO will work as. As only two bits are available only a max of 4 choices can be used.
But as you can see in a few pins there are a more than 4 functions for a few…
Part Number: MSP430FR5857 Tool/software: Code Composer Studio Hey.
I am running a code and I get the following optimization advice.
Can someone tell me what the problem is and how to eliminate it?
#include <msp430.h>
static unsigned int var =0;
static…
Part Number: MSP430FR5857 Tool/software: Code Composer Studio Hey,
This question might seem a little childish but hear me out.
Each bit in each PxIN register reflects the value of the input signal at the corresponding I/O pin when the pin is configured…
Part Number: MSP430FR5857 Other Parts Discussed in Thread: MSP-GRLIB Tool/software: Code Composer Studio Can anyone tell me where I can get Graphics library for I2C and SPI displays and any examples related to them?