Other Parts Discussed in Thread: MSP430FR5859 Hi There,
I am having an issue with MSP430FR5859 and its I2C in slave mode.
Like the screenshot below, when repeat start is issued immediately after MSP430FR5859 acks, MSP430FR5859 will hangs. It may not happen…
I am trying to run a project from the ti driverlib examples (Code provided below). The code sets the DCOCLK to 16Mhz, then sets the MCLK and SMCLK to reference the DCOCLK. When the MCLK is set to reference the DCOCLK, an interrupt is hit at 0xFFFA (User…
Other Parts Discussed in Thread: MSP430FR5739 , MSP430FR5859 I have existing boards designed for the msp430fr5739. Can I use the new msp430fr5859 as replacement dropins?
carl
Part Number: MSP430FR5994 Other Parts Discussed in Thread: MSPDS , ENERGYTRACE , MSP430FR5859 Hi,
I am using MSPDS open source package v3. So far I was able to capture the device current, voltage and energy measurements using time driven profiling (ETMode…
Other Parts Discussed in Thread: MSP430FR5859 , MSP430WARE Hi,
I'm using MSP430ware to create 4 continuous mode TimerA on MSP430FR5859 chip.
All timers were working fine, however when I change timer1 to UpMode, timer2 and timer 3 does not interrupt…
Other Parts Discussed in Thread: MSP430FR5859 Hi all,
I am trying to use the UCTXIFG and UCTXCPTIFG flags to determine when the UART has finished transmitting some data I have sent (using DMA to transfer from memory to the TX buffer but I don't suppose…
Other Parts Discussed in Thread: MSP430FR6989 , MSP430FR5859 Hey everyone,
I am working on a new project and I would like everything, main code, variables, stack, etc to be inside the FRAM on the MSP430FR6989. Currently, if I put all the of the variables…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…