Part Number: MSP430FR5962 Hi Expert,
One customer is using MSP430FR5962 in a humid environment and finding the controller can't work well. Open the casing, there are some condensation on the internal casing surface but no obvious water drops can be seen…
Part Number: MSP430FR5962 Dear All,
Is there any detailed ADC information (characteristics) available when using the
internal voltage reference VREF = 1,2V
where also the conversion result is compensated with the calibration values from the TLV structure…
Part Number: MSP430FR5962 Dear MSP champs,
Looking at the Crypto-Bootloader (CryptoBSL) for MSP430FR59xx and MSP430FR69xx MCUs datasheet , it seems that the CryptoBSL source code is only available within IAR project environment. Having in mind that the…
Part Number: MSP430FR5962 Hi Forum
I have some questions regarding the SPI
I have an application where we run a SPI at 8Mhz, MCLK is 16Mhz. Compiler is CCS.
Now I want to send data and receive back to back to back, but it seems to be a problem. I have…
Part Number: MSP430FR5962 Hi Forum
I have a problem clearing the GPIO interrupt. I have enabled PORT3 pin 3 interrupt.
P3DIR &= ~( BIT3 ); P3OUT |= BIT3; P3REN = BIT3; /* Select pull-up mode for interrupt input */ P3IES = BIT3; /* Hi/Lo edge */ P3IFG…
Part Number: MSP430FR5962 Hello all,
I'm trying to use the repeated autoscan mode on the MSP430FR5962. I'm having a few issues getting the feature working. After all of my attempts I have not been able to get the module to work correctly. Sometimes the…
Part Number: MSP430FR5962 I have a few #if compiler options in my code to handle some if-else branching depending on the options for a protocol stack.
When using the IDE to perform brace matching to identify blocks, the non-compiled branch (e.g., #else…
Part Number: MSP430FR5962 Hello experts,
Could you tell me shelf life of MSP430FR5962IRGZ?
I would appreciate if you would tell me shelf life before and after opening package, if possible.
Thanks and best regards,
Ryo Akashi
Part Number: MSP430FR5962 I have some very strange behavior going on and I'm not able to pinpoint why exactly it's happening. Everything runs exactly as expected in both release and debug configurations with the FET attached. However, on a debug…
Part Number: MSP430FR5962 Hi,
I would like to have the clock output from the IO port of MSP430FR5962.
Q1:Can the IO port of MSP430FR5962 output a 4MHz clock? Datasheet specifies the minimum value of the clock output as 16MHz, but could it be a mistake…