Part Number: MSP430FR5964 Could I confirm if the RTC DayOfWeek is validated in any way (other than the obvious 0-6 value). I'm specifically interested if anything is done to ascertain that the DayOfWeek really complies with the year, month and Day…
Part Number: MSP430FR5964 A couple of weeks back I was working through a code composer issue where multiple break points were being generated for a single (C) source line This was subsequently resolved by migrating the build optimization level from -O0…
Part Number: MSP430FR5964 Other Parts Discussed in Thread: MSP430F2618 Hello everybody,
my MSP430FR5964 runs at 2.8 V.
Now I am looking for a way to trigger an interrupt if the supply voltage VCC falls below 2.5 or 2.0 V.
With the MSP430F2618 you had…
Part Number: MSP430FR5964 Other Parts Discussed in Thread: MSPWARE , MSP430FR5994 Since I've upgraded to CCS 10.4, I've had a few cases where resuming from a breakpoint doesn't appear to do anything, until it is resumed a second time.
In all…
Part Number: MSP430FR5964 I've been having a play with the NVS utility in the MSP MCU FRAM Utilities, and almost have it working as expected, but not quite! The NVS data is being correctly being positioned in FRAM, and retained on restarts, but if…
Part Number: MSP430FR5964 Other Parts Discussed in Thread: MSP430F149 , I am in the process of migrating my code from a old MSP430F149 to a new MSP430FR5964. As this newer processor has more IO and more RAM, there is less space for code in the first memory…
Part Number: MSP430FR5964 Hi experts,
Please let me confirm the following description of SVSHIFG in "2.3.3 PMMIFG Register" of the User's Guide.
Q1:Is it correct that "high-side SVS levels" means SVS H_IT+ and "brownout levels" means SVS…
Part Number: MSP430FR5964
I've just starting tripping over a problem I've never seen before, and I'm struggling to understand what is causing it.
Normally on reload or startup, the code automatically breakpoints at the main() entry point…
Part Number: MSP430FR5964 Hi experts,
My customer is evaluating the MSP430FR5964. When they add a symbol for external reference in the linker command file and build with reference from C source file (inline assembler), they sometimes get an error (Undefined…
Part Number: MSP430FR5964 Other Parts Discussed in Thread: UNIFLASH , MSP-FET We are encountering an issue that appears to be parts of the MSP430FR5964 FRAM being corrupted when power is cycled to the device.
The linker memory segments are defined as follows…