Part Number: MSP430FR6043 Other Parts Discussed in Thread: MSP430FR6047 , TDC7200 Hello, I wish to implement a smart water-meter.
the requirements listed below :
It must be possible to measure water flow accurately 20-320 liters/h - <5% error 320…
Sorry, I don't know about HTTP POST or Curl. You are doing a work purly to convert the message into a HTTP post structure. I think it is a purely software work and have no relationship with the MCU. I would ask you try to ask internet or chatgpt. It will…
Hi,
Cheska Abarro said: I meant the 3.3v on the J5 is not working.
Have you checked if there is jumpers on the J30? If not, you need to add jumpers on it.
Cheska Abarro said: I also tested the power the board through J33 pin but I also did not get any measurements…
Part Number: MSP430FR6043 When building for MSP430FR6043 with "-mcode-region= none " we can use start/end markers surrounding each section in the linker script to calculate per-sections' CRCs in a post-build step.
Example from msp430fr6043…
Part Number: MSP430FR6043
Hi Team,
There's an issue from the customer need your help:
1. I want to achieve the following functions:
The EV kit consists of two channels, J5 and J6, where J6 (UPS) detects the distance to the active target, J5 (DNS…
Part Number: MSP430FR6047 Other Parts Discussed in Thread: MSP430FR6043 Hello,
I am currently using MSP430FR6043 for gas metering using the MSP430FR6043EVM_USS_Gas_Demo application. However, I am having some challenges due to limited FRAM memory space…
Part Number: MSP430FR6043 Hi Team,
My customer cannot find the implementation of the function USS_generateMultiToneBinaryPattern , we can only find the statement in UssSwLib.h . Could you please point the location to us?
--
Thanks & Regards
Part Number: MSP430FR6043 Question 1: The customer is using the MSP430FR6043 ultrasonic gas meter solution. The customer is testing the 6000V electrostatic discharge test and finds that the external 32.768K clock output is normal and the serial port baud…