Part Number: MSP430G2121 Other Parts Discussed in Thread: MSP-FET Can I double use the JTAG and SPI. I am looking at the MSP430G2121 for a design, it has TCK,TMS,TDI,TDO on the same pins as SCLK,SDO,SDI.
Does the part know to mux functionality between…
Other Parts Discussed in Thread: MSP430G2121 Hello,
I have a MSP430G2121 and I don't understand if it has internal Low Clock.
I want to have MCLK and SMCLK ~= 0.1 MHz and ACLK ~= 10kHz with no additional components like quartz.
Is this possible ? How…
Other Parts Discussed in Thread: MSP430G2121 I am trying to create working SPI code for the MSP430G2121. I am referencing the example code provided by TI and using a logic analyzer to read the values on the MOSI and MISO lines. However, when I flash the…
Other Parts Discussed in Thread: MSP430G2121 , MSP430G2153 , MSP430G2203 , MSP430FG4618 The Msp430g2121 has SPI ... don't see an STE input ... needed to make the device an SPI slave. Am I missing something?
Joseph Olivier said: Do I need something else? No, you don't need anything else. However, you may use the MSP430 Flasher command line utility program as well. It can be used to download your application.
Part Number: ADS1298RECGFE-PDK Other Parts Discussed in Thread: MSP430G2121 , ADS1298R Hello,
We are working on ADS1298R we has Ref. Board now we want to design custom hardware so we have some doubt in the Reference design The MSP430G2121 (MCU) use with…
Other Parts Discussed in Thread: MSP430G2121 , DAC5311 hello,
Connection between MSP430G2121 and DAC5311.
I encouter some incorrect reading, at per below:
1) 0 bits - reading: full voltage of 3.3v ,
2) 255bits - 0V
3) 50bits to 200bits - voltage reading…
Part Number: ADS1298RECGFE-PDK Other Parts Discussed in Thread: MSP430G2121 , TLV3491 , ADS1298R Hello,
We are working on ADS1298R we has Ref. Board now we want to design custom hardware so we have some doubt in the Reference design The MSP430G2121(MCU)…
Other Parts Discussed in Thread: DAC5311 , MSP430G2121 Hello,
Can you pls help to verify the below code to transmit from MSP430 to DAC via SPI.
Task: to transmit 8-bits data from MSP430 to DAC5311 when there is a change in duty cycle.
Issue: The output…