Other Parts Discussed in Thread: MSP430G2121 , MSP430G2153 , MSP430G2203 , MSP430FG4618 The Msp430g2121 has SPI ... don't see an STE input ... needed to make the device an SPI slave. Am I missing something?
Other Parts Discussed in Thread: MSP430G2153 Hello,
I'm planning to use the MSP430G2153 and want to make sure that in using the USCI for both the I2C and UART function, that both of these are supported simultandiously and also that that I can also still…
Sascha W. said: There is a Timer B on MSP430G2153,.. or not? The data sheet says... no. Just two TimerA with three CCRs. (which is more than the other G series MSPs with only one TimerA with two CCRs)
Hi Andreas,
We are facing the same "unknown device" problem.
Is there any patch for the MSP430G2153 device?
We are using the CCSv5.1 and the MSP-FET430UIF tool.
Thanks in advance,
Andre Fernandes
Other Parts Discussed in Thread: MSP430G2153 I'm receiving two Compilation failure and I am not sure how to resolve.
error: option --optimize_with_debug is missing its parameter 'on,off'
fatal error #10192: Failed linktime optimization
I just…
Hi,
We are in a hurry to deliver a project.
The firmware is almost finished but we are not able to programming.
I have already tried with CCSv5.1 and v4.2 and two program tools, the MSP-FET430UIF and MSP-EXP430G2.
The power is supplied from the FET…
Other Parts Discussed in Thread: MSP430G2153 In Grace 1.0, if after opening the ".cfg" file in the Grace user interface, the Grace Outline tab is closed, changing of many of the ComboBox selected items in many of the device peripherals is ignored.…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…