Part Number: MSP430G2253 Other Parts Discussed in Thread: MSP430F5529 , MSP430G2553 , MSP430FR5969 , LMP91000 Hi
I want to use a couple of MAG3110 and it can only communicate using i2c. But I can't change the address. Is there any way to communicate with…
Part Number: MSP430G2253 I am trying to do a simple light up the entire display after the intialization, but my code doesn't seem to work. any suggestions on debugging the issue? (have no logic analyzer or oscilloscope yet)
/********************…
Part Number: MSP430G2253 Other Parts Discussed in Thread: MSP430WARE , MSP430G2553 Tool/software: Code Composer Studio In particular would like to have non-grace example projects for SPI and serial communication. This used to be part of CCS. Now I can not…
Other Parts Discussed in Thread: MSP430G2553 , MSP-FET Tool/software: Code Composer Studio Hey there!
I've got problems using my MSP430G2553 Launchpad on my new machine (Win10 - MSI Z97 G55SLI - Intel I5 - CCS 6.2). I often get " No USB Fet was found" and…
Other Parts Discussed in Thread: MSP430G2253 We are using the 2253 in an automotive application that is capable of experiencing temperatures in excess of 60C. When the temperature rises above 50C, the processor resets and continues to do so at approximately…
hello there here it is my code for adc and uart. in code variable a,b,c make digit which is i am transmitting through UART. now i want to set threshold like if value is less than 1.9 then i want to turn on LED .but it doesn't work for me.
i am asking…
Other Parts Discussed in Thread: MSP430G2553 hi ! if i want to make wireless signal acqusition system using HC05 bluetooth. i want to use just msp430g2553 ic instead of launchpad. how can i do it?i have interfaced hc05 bluetooth with msp430g2553 launchpad…
Hi Charles,
The EP notation stands for enhanced product. Essentially, this means there are some enhancements compared to the original MSP430G2230 such as a wider operating temperature range.
If you don't need this feature, then I would recommend taking…
I have no idea what SlickEdit is but defining a symbol is not the usual way of telling GCC which device you are using. Use -mmcu= instead. As in:
make -k
/usr/ti/gcc/bin/msp430-elf-gcc -g -mmcu=msp430g2253 -I /usr/ti/gcc/include -Wall -Wl,--gc-sections…