Other Parts Discussed in Thread: MSP430G2253 Hello.
I need to generate pwm on pin 2.3 of msp430g2253. for example,with 75% duty cycle.
I have rewritten example program from the package.But I have scaned pin 2.3 via oscilloscope. There weren't any result…
Other Parts Discussed in Thread: MSP430G2253 , ADS1240 Hello!
I need comminucation between ads1240 and msp430g2253 devices through spi.
I use 4 pin connection . I have written code to initialize spi on msp430.but when i try to transmit command to ads and…
Hello!
I need comminucation between ads1240 and msp430g2253 devices through spi.
I use 4 pin connection . I have written code to initialize spi on msp430.but when i try to transmit command to ads and then receive response through spi, i have nothing.
can you…
Other Parts Discussed in Thread: MSP430G2253 Hello,
I'm using IAR Workbench ver. 5.30.1; the device MSP430G2253 is included. But I still get the message "Fatal error: Could not find device (or device not supported)". I've tried #include <msp430.h>. But…
The following is what I'm doing now. I tried to do this without the delays. If I was going to use interrupts, do I still need to build in the delays? Is there anyway to remove the delay completely?
I'm completely aware this code is probably horrid…
Part Number: MSP-EXP430G2ET Other Parts Discussed in Thread: MSP430G2253 , Tool/software: Code Composer Studio Hello, I am new on programming MSP430 and work at the moment with the MSP430 Launchpad MSP-EXP430G2ET with the MCU MSP430G2253 on it. I have average…
Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP430G2253 Tool/software: Code Composer Studio Dear Buddy:
Current I did building LCD1602 Display by 4 bit.
But I met failure which it can not display anymore.
MSP-EXP430G2 Emulation Board connect…
Hey James,
My project leader insists on the MSP430G2553. I was looking at the source code from www.ti.com/.../slva557.pdf and all of the relevant source code I could find on the parts homepage. I also found the TIDA-01496 reference design that is very…
Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP430G2253 Hello everyone,
In msp430 ,how much delay it generates if I write the statement __delay_cycles(1000).Is that mean 1ms delay because by default msp430 works at a frequency of 1.02MHz…
Part Number: FDC2214 Other Parts Discussed in Thread: FDC2114
Dear Team,
We have procured The MSP-CAPT-FR2633 : MSP CapTIvate MCU Development Kit.
We wanted to measure the RAW / Absolute capacitance value (in pF ) using the capacitance sensor.
But, usi…