Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP430WARE Hi,
We are trying to interface 1.54" EPD with MSP430G2553LP. We have IAR code with us. here i am sharing the code file for reference.
// #include "io430.h" #include "msp430…
Part Number: MSP430G2553 I'm trying to upgrade the MSPG2553 using the steps outlined in this support ticket: https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/991977/msp430g2553…
Part Number: MSP430G2553 Other Parts Discussed in Thread: PCF8574 I'm a starter, I'm in need of an example code for displaying data on the 16x2 LCD with MSP430G2553 communication through I2C with PCF8754 module.
Part Number: MSP430G2553
Hello, I want to create 2 different PWM signals of 10 kHz with MSP430G2553. DUTY cycle value of PWM signals is 50% and fixed. Two different potentiometers are connected to the microprocessor and these potentiometers are responsible…
Part Number: MSP430G2553 Hello everyone. Good morning, I need help with the MSP430G2553 and the E32 LoRa module. I have the code below, but I'm not sure why it isn't working. Could someone assist me with some tips? . Manual link: www.manualslib…
Part Number: MSP430G2553 Hello, sorry for the stupid question but somehow I stuck in the mud. I like to enter BSL on a simple launchpad (final app will use FR6047 but for simplicity I take the launchpad) from an ESP32s Serial (first image). I connect…
It has been 3 weeks since I first posted and I have yet to receive any support from a TI employee. As far as I can tell, this is the only way to get support from TI unless I go through side channels to get connected with an FAE, which it seems like I…
Part Number: MSP430G2553 I designed a board using the MSP430 interfacing with a computer using an FTDI uart to usb converter. I'm accessing the bsl using GPIOs in bit bang mode and then programming the device using the deprecated BSLDEMO . When programmed…
Part Number: MSP430G2553
Dear TI Experts,
I have a problem with configuring four-pin mode here for MSP430G2553 launchpad. I was able to transmit and receive data through UCA0 3-pin SPI channel, but I now need to use 4-pin SPI channel which includes…
Part Number: MSP430G2553 我购买的单片机型号为MSP430G2553,在MacBook上的Code Composer Studio 12.4.0软件上运行编写好的代码,代码本身没有问题。将单片机连接到电脑上后,需要将代码烧录到单片机内,结果Code Composer Studio 12.4.0软件弹出如下错误:
MSP430: Error initializing emulator: No USB FET was found
可以看出来电脑没有识别出单片机。我的 Mac…