Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP430FR2475 , , MSP430G2402 TI Friends and Family,
Our customer has found a peculiar anomaly between ID Codes on FR2475 and targeted G2553. Comments welcomed!
[Customer}
I am getting our manufacturing…
Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP-FET I am attempting to flash my target with the MSP-FET and the IAR IDE MSP430 v8.10.2.
I have tried both with power supplied from the target and from the MSP-FET
I am getting the error: "Device…
Part Number: MSP430G2553 As stated in title, I am using P1.1 and P1.2 to trigger the PORT1 interrupt service routine, triggering on the down edge. See screenshot for incoming waveform down edges.
They're about 3 microseconds apart in this case. When…
Part Number: MSP430G2553 So we are using msp430 for one our application for deugging purpose iwant to use printf instead of uart so while i used printf function iam getting the following error how can i resolve it, as i am new to ccs studio please gu…
Part Number: MSP430G2553 Hello, I am trying to get my head around how the Timer0 interrupts work.
I am not posting my code because after many tries it is not quite tidy, but I can post if needed. What I am trying to do is count the RPM of a motor, for…
Part Number: MSP430G2553
Hi Team,
There's an issue from the customer need your help:
What is the maximum input and output current of the IO pins allowed by the MSP430G2553 microcontroller? Where is it reflected in the chip manual?
Thanks & Regards…
Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP-EXP430G2ET
Hello,
we use the "old" MSP-exp430G2 with CCS10.4 to debug the MSP430G2553-20PIN and the MSP430G2452-14PIN.
This works very well.
The MSP430G2553-28PIN has now been…
Part Number: MSP430G2553 I am trying load the firmware to MSP430G2552, Is there other way to load the firmware even though fuse blown. when I am trying to access its showing as below.
Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP-GANG , MSP-FET , MSP-FLASHER Dear sir/madam,
We are using MSP430 and TM4C129ENCPDTI3R microcontroller for our new development project. With in next few months we plan to release the project…