Part Number: MSP430G2744 Hi Team,
My customer wants to use the timer A3 in Up Mode and has a few questions listed below.
As it says in SLAU144J 12.3.1 TACTL bit5-4, "01 Up mode:the timer counts up to TACCR0.", is it correct that to use the timer in up…
Part Number: MSP430G2744 Hi Team,
My customer has a few questions regarding the ADC10. They are using the MSP430G2744IRHA40R.
1. Regarding the ADC10CTL1[15:12]INCHx, on the Family User's Guide, it says that A12-A15 are only able to be used on MSP430F22xx…
Part Number: MSP430G2744 Hi Team,
My customer has a few questions surrounding the interaction between PUC and Digital I/O ports.
When PUC is triggered, are the digital I/O ports set to 0? On the Family User's Guide, it shows the table below, where the…
Part Number: MSP430G2744
Hi Team,
I have a question regarding the specific condition to classify a oscillator fault.
I see in the datasheet under 5.20 Crystal Oscillator LFXT1, Low-Frequency Mode, there is an oscillator fault frequency MIN and MAX value…
Part Number: MSP430G2744 Other Parts Discussed in Thread: UNIFLASH , MSP-FET , , MSP430F2272 Ubunutu 20.04
CCS 11 / Uniflash 7.2
MSP-FET, Tag-Connect SBW connection to custom board.
I cannot flash or debug my custom target board based on the MSP430G2744…
Hi, There was no feedback since a while, so I assume this tread is resolved and can be closed. You can still reply to this thread after it is closed, or you can create a new thread. Best Regards, Andreas.
Part Number: MSP430G2744 Hi,
-We are using msp430g2744 as qwerty keypad controller in our android based laptop.
I got the firmware code for the same from below link.
https://www.ti.com/tool/TIDM-KEYBOARD
I have built it and flashed in our board's msp430g2744…
Part Number: MSP430G2744 Other Parts Discussed in Thread: MSP430G2553 Hi Team,
Our customer would like to get the checksum for the MSP430G2744. I understand from the E2E thread below that get the checksum using the Elprotronic FET-Pro430.
https://e2e.ti…
Part Number: MSP430G2744 Hi,
We are planning to use MSP430G2744 for interfacing with standard PC keyboard over USB or I2C.
We have few queries on the same. The keyboard that we are planning to use is below.
Can we have both I2C and USB interface option…
Part Number: MSP430G2744 Hi Team,
Customer encountering problem regarding the IEC60730_system_config.h. and they using msp430_iec60730_software_package_1_20_00_03. Below is the inquiry.
"
I put the IEC60730 into the program, but complier shows error…