Part Number: MSP430I2040 Hi,
I am trying to save a large chunk of data, a struct for some user generated settings, into flash to persistent them. The size if 112B. Somehow sometimes only the first 3x ~ 10x bytes are actually saved when read back the entire…
Part Number: MSP430I2040 We are using MSP430I2040 EVM ( https://www.ti.com/lit/an/slaa638/slaa638.pdf) for metering application development. We want to measure the maximum 32A current.
1) Is it possible to measure 32A current via shunt provision available…
Part Number: MSP430I2040 Hi,
we want to order the EV board for MSP430I2040 as in attached pdf.
we only find the EV board MSP-TS430RHB32A but this is not the Solution for Thermopile sensor as below:
sboa501.pdf
can you please support with this EV board…
Part Number: MSP430I2040
Hi team,
Here's the issue from the customer may need your help:
The flash for the MSP430I2040 written in the manual is 16KB, then the storage address is 0xffff-0xc000.
But the MSP430I2040 in hand can execute code from 0x8000…
Part Number: MSP430I2040 Hi,
I was working on a project based on MSP430I2040. While trying to figure out why the initial code didn't work as expected, I removed various parts of the code, then built and downloaded into MCU. After a while, I found out…
Part Number: MSP430I2040 Hi,
I am trying to save some user generated settings into information flash(the section starts at 0x1000), because some device specific TLV data also exists at the end of this section (starts at 0x13C0), we will need to read that…
Part Number: MSP430I2040 Hi,
We are trying to integrate revenue grade energy metering into our solution.
Is this part MSP430I2040/2041 suitable for meeting this requirement?
Thanks,
Preveen
Part Number: MSP430I2040 Looking for the micro-controller that can measure the AC supply both power and energy with 2% accuracy.
Max pin size 28 - 32 package and having small footprint.
Planning to use metering feature in LED driver. We want to provide…
Part Number: MSP430I2040 Other Parts Discussed in Thread: UNIFLASH Hi MSP430 Experts,
What would you expect to happen if we tried to write flash into an area of flash that doesn’t exist on the part. For example if we write our program code into…
Part Number: MSP430I2040 Other Parts Discussed in Thread: MSP430I2041 I generate default code from EnergyMeasurementDesignCenter tools with chip select MSP430I2041. After generated code compile with CCS and change target chip to MSP430I2040. Load code…