The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: MSP430I2041 Other Parts Discussed in Thread: MSP-FET , , UNIFLASH My customer wants to load image to MSP430i2041 using MSP-FET and FET-Pro430(ver. 3.4-1). But it failed at verify process. If they use UniFlash (v.8.1.1), verify is OK, but it does…
Hello Yoo,
I have done some tests on my side today using the MSP430I2041. And I can download the txt file you sent to me successfully. The actual size is 27128 bytes. Maybe you need check your own hardware connection, including the JTAG/ SBW interface…
Part Number: MSP430I2041 Hello,
I want to design a system that allows me to measure very low currents, in the order of micro-amperes, with decent accuracy, let's say with a maximum error of approximately 1%. I've been exploring some ideas, and I thought…
Part Number: MSP430I2041 I am using MSP430i2041 to create a device that requires OTA(over the air) upgrade functionality, but I have not done it before. Do you have any relevant routines or application notes provided.
Part Number: MSP430I2041 I want to use this microcontroller in a weight scale and what I notice that its maximum gain is 16, but also it include oversampling, so I want to know if I can optimize the oversampling to improve the gain as I want the gain…
Part Number: MSP430I2041 Hello i am trying to implement a RS485 Interface with an MSP430 using the eUSCI modul and a RS485 tranciever. There i noticed a unexpected behavior by the UCTXCPT Flag/Interrupt and also some weird wording in the MSP430i20xx User…
Part Number: MSP430I2041 Hi Team,
simulator: MSP-FET430UIF
software:
The simulator can not connect with the target, and can not download the program. Here is the error information:
JTAG communication initialization.... failed
Verifying Security Fuse…
Part Number: MSP430I2041 Other Parts Discussed in Thread: MSP430I2040 , Hello,
a general question about the i2041. Is it suitable to measure thermocouples or are there any better suited MCU with 16/24Bit ADC in the same size?
Get your point, sorry, we don't have this parameter. See from the datasheet, the max mismatch, should be lower than 4%. If you want to reach higher accuarcy, I would suggest you do calibration.