Part Number: MSP432E411Y Other Parts Discussed in Thread: UNIFLASH , Hi
My customer is trying unlock MSP432E4's JATG for change MAC address.
Now, trying this sequence using XDS560v2, but doesnot works.
https://e2e.ti.com/support/microcontrollers/arm…
Hi Ki,
Thanks for supporting,
Ki said: This function is defined in the msp432e411y.gel file. Is the customer using this gel file with their target configuration?
Might be Yes,
My customer set to using debug probe to XDS560v2 in target configration.
Ki…
Part Number: MSP432E411Y Other Parts Discussed in Thread: UNIFLASH Hi
May I have question about MSP432E411Y USER_REG0 register?
In TRM, We could change 1 to 0 the USER_REG0 to USER_REG3 Registers.
And there is only way to reset this register is 3.3.4.3…
Part Number: MSP432E411Y-BGAEVM I am looking for the complete design files for this eval board.
I would like the BOM, PCB fabrication drawing and gerber fiels.
I have not been able to locate these on the site.
Could someone please help me with this…
Part Number: MSP432E411Y Other Parts Discussed in Thread: UNIFLASH I have installed UniFlash 8.5.0 on Ubuntu 20.04 LTS, and while it launches and runs, if I try to program a part, as soon as I click on "Load Image",
a red error bar appears at…
Part Number: MSP432E411Y Other Parts Discussed in Thread: MSP432E401Y
Hi,
We are considering migrating the TcpEcho sample code provided based on MSP432E401Y to MSP432E411Y.
Due to the different packaging, we believe some software changes will be required…
Part Number: MSP432E411Y Hi,
I will develop communication module with DLMS/COSEM protocol of gas metering by using MSP432 and found that TI has DLMS/COSEM library to support.
Please check and confirm update library and to get access.
Thanks,
Manop
Part Number: MSP432E411Y Hello,
Are there routines to support the MSP432E4xx RTC clock? I'm looking for a function similar to the MSP432P4xx's RTC_C_getCalendarTime(). If not, can I use the routine time() specified in time.h?
Best,
Magda
Part Number: MSP432E411Y-BGAEVM In the Eval board design, the USB connector has a power pin, labeled TARGET_VBUS and this is connected to pin B16, USB0VBUS.
In my my design, I am using the processor as a device, not a master, in that power is coming…
Part Number: MSP432E411Y Could someone provide an example of using the QSSI interface to connect up to a simple device such as the Microchip 25LC640T-I/SNCT-ND?
Thanks.
Clyde