Hi Sylvain,
It's been a while since we have heard from you, so I'm going to assume you were able to move forward with your project. I will mark this posting as RESOLVED, but if this isn’t the case, please click the "This did NOT resolve my issue…
Part Number: MSP432P401R Hi
I was looking at the memory map for the above processor.
I was wondering if the "Unused" memory from 0x6000_0000 to 0xDFFF_FFFF was available for storage by a program that I have developed.
I have a lot of data to…
Hi,
I am using the MSP432P401R for programming a DDS (AD9833). When I program it with the UCB0CLK and UCB0SDA, there is no problem, I can do it.
But these pins are used for something else and I tried to program the DDS with the UCB1CLK and UCB1SDA instead…
Part Number: MSP432-RTOS Other Parts Discussed in Thread: CC3120MOD , BOOSTXL-AUDIO , CC3120 Hello,
I am working on a college project where I want to use the CC3120MOD along with the BOOSTXL-AUDIO to wirelessly transmit sampled audio data using an MSP432P401R…
Part Number: MSP432P401R Hello,
I am using a MSP432P401R and a CC2564 to form a bidirectional SPP <-> UART bridge. For the HCI UART I am using the provided HAL (baud rate 2000000) and for the Host UART I am running at 921600 and have implemented hardware…
Part Number: MSP432-RTOS Configuration :-
1) Using MSP432P401R& TI's MSP-FED Flash Emulation Tool
2) Using CCS for dev. Got a Custom BSL and an application code
3) Need to perform "ERASE_TOTAL" and then flash the image is generated as TI…
Hello Jayden,
Check out the following app note for some general UART debugging tips to get you started: Solutions to Common eUSCI and USCI Serial Communication Issues on MSP . Its titled focused on MSP430, but the MSP432P4 has the same eUSCI module.
You…
Part Number: MSP432P401RMSP432P401R JTAG/SWD LOCK
Trying to issue a factory reset command to the MSP432P401R chip to unlock the chip.
Just tried the method mentioned by somebody in the forum, which is this:
MSP432E4 SimpleLink Microcontrollers Technical…
Part Number: MSP432P401R Hello,
Please point me to the Schematic and BOM for the MSP432P401R Launchpad board. In particular, I'm interested in the P/N for the switches use.
Regards,
-david
Part Number: MSP432P401R Hi
In the user documentation it says that J6 can be used as an external 3.3V source. Can J7 be used as an external 5V source? I could not find a description for J7.
My goal is to find out if I can supply a 5V source to the board…