Part Number: MSP432P401RMSP432P401R JTAG/SWD LOCK
Trying to issue a factory reset command to the MSP432P401R chip to unlock the chip.
Just tried the method mentioned by somebody in the forum, which is this:
MSP432E4 SimpleLink Microcontrollers Technical…
Part Number: MSP432-RTOS Configuration :-
1) Using MSP432P401R& TI's MSP-FED Flash Emulation Tool
2) Using CCS for dev. Got a Custom BSL and an application code
3) Need to perform "ERASE_TOTAL" and then flash the image is generated as TI…
Part Number: MSP432P401R Hello,
Please point me to the Schematic and BOM for the MSP432P401R Launchpad board. In particular, I'm interested in the P/N for the switches use.
Regards,
-david
Part Number: MSP432P401R Hi
In the user documentation it says that J6 can be used as an external 3.3V source. Can J7 be used as an external 5V source? I could not find a description for J7.
My goal is to find out if I can supply a 5V source to the board…
Part Number: MSP432P401R Hi all, the idea of this little program is to be able to read the value of a potentiometer using the ADC of the MSP432P401R. To get a more accurate measurement I calculate 4 values and average them and assign them to the variable…
Part Number: MSP432P401R Hi Support Team ,
Regarding the MSP432P401R and BOOSTXL-CC3120MOD , I would like to know the following questions.
MSP432P401R as External MCU and BOOSTXL-CC3120MOD as NWP
and I measure the current in Always connected mode the…
Part Number: MSP432P401R Hi, the idea of the project is to detect the Back Electromagnetic Force (BEMF) of a BLDC and for this I have made this simple program where I wanted to use the ADC of the MSP432P401R in differential mode, since I have used six…
Part Number: MSP432P401R Hello, my project idea is to rotate a BLDC motor by imposing a certain duty cycle value (which I change with Launchpad buttons) and setting a period value (in this case 1 ms) that allows me to make transitions between 6 states…
After changing the DCO frequency the following error started appearing: CORTEX_M4_0: Error initializing flash programming: Your XMS432P401R material is no longer supported. We recommend you moving to production-quality MSP432P401R/M silicon by ordering…
Hello,
After isolating portions of the code used for transceiver mode, I have found the source of the issue.
There were a couple lines inside my transceiver functions that allowed a successful connection to occur after exiting. They are attached below…