Part Number: MSP432P4111 Hello, I have encountered some issues with using I2C in out application. I would like to connect a TCA8418 to a MSP432P4111 via I2C in fast mode (400 kHZ). According to the datasheet, the TCA8418 requires 0.6 us for I2C clock high…
Part Number: MSP432P4111
In the related thread , Crazy Eng asks: " How to use and implement Hwi, Swi, Tasks modules with MSP432 in CCS v10".
James points to the SImpleLink Academy as a good way to get started. You may also want check out the Getting…
Part Number: MSP432P4111 My design has both MSP430 and MSP432 on the board, previously I am using MSP-FET and J-Link Base to program them, it works, for some reason, I plan to use MSP-FET-432ADPTR to replace J-Link Base, however, the SWO is not connected…
Part Number: MSP432P4111 Hi,
I'm using the idle task for logging data out UART from both LoggerIdle and SysMin, so I need to add a mutex to synchronize the two streams so the data isn't interleaved. This is fine and works well, but I specifically need…
Part Number: MSP432P4111 HI,
I am trying to initialize P55/A0 P54/A1 P53/A2 P52/A3 as ADC channels with the below code while initializing P54/A1 channel gets connected to the ground.
WDT_A->CTL = WDT_A_CTL_PW | WDT_A_CTL_HOLD; volatile unsigned int…
Part Number: MSP432P4111 I'm working with multiple coding partners using multiple hosts computers, all using the same code base.
The code builds on CCS v10 for windows and max osx but not ubuntu.
What is helpful is that you don't need the entire code…
Hello Sasi,
I'll assume you were able to resolve your issue so I will go ahead and close this thread. If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information. If…
Part Number: MSP432P4111 Hi,
I am working in a custom board developed for msp432p4111 the controller was working fine, i tried to debug a sample code for uart protocol now i am getting an error "Error connecting to the target: Unknown devic"…
Part Number: MSP432P4111
We've been trying to track down an issue that occasionally occurs in our system. Following it down in Clock.c within Simplelink 3.40.1.2, we notice that the issue occurs when the ticksToService in Clock_workFuncDynamic returns…