Part Number: MSP432P4111T Hi,
I have a system where there are multiple MSP432. Each MSP432 needs to be loaded with different program. I am using XDS110 to JTAG programming. I don't want to take out multiple JTAG cables out of the system. I want to know…
Part Number: MSP432P4111 Hi,
Is the MSP432P4111 T pin compatible w/ the MSP432P4111? Other than differences in the maximum clock rates and operating temperature, are there any other differences?
Thanks,
Erik Thompson
Part Number: MSP432P4111T I would like to know whether MSP432P4111IPZ supports live firmware update in the field similar to dsPIC33CK256MP508 or STM32L471VET6 ?
If not is there a TI any other TI part supports this feature.
Part Number: MSP432P4111T Hello , i want to make a project with MSP432P4111T (MCUs 32 bits with a 2MB Flash and 256 KB of SRAM) with a TFT LCD Display (262K Colors), my quastions is : please can you tell me which is the best LCD display screen (Without…
Part Number: MSP432P4111T Team,
My customer has the following question:
Regarding MSP432P4111T device, why is the lowest storage limit only -40⁰C and not -55⁰C or -65⁰C, typical for active devices?
Regards,
Aaron
Part Number: MSP432P4111T Our proposed architecture in our board is as given in the figure below. We are having 2 system controllers - one is primary and one is redundant. The primary controller is MSP432P4111T. What we are planning to do is as given…
Part Number: MSP432P4111T I believe that the MSP432P4111 SimpleLink™ Microcontroller LaunchPad™ Development Kit (MSP-EXP432P4111) User Guide has swapped J1 and J3 on page 20.
The silkscreen is correct and corresponds to the design guide .
Part Number: MSP432P4111T I am using the MCU MSP432P4111TPZ in my design with AVCC, DVCC at 3.3V. I need the Vih, Vil, Voh and Vol of various interfaces (SPI,I2C, UART, GPIO) in MSP432P4111TPZ. It is not given in datasheet. Please reply soon since it…
Alternatively, will the following MCU run with the following WiFi and Bluetooth modules, with the associated SDK plug-ins, using IAR Workbench?
MCU: MSP432P4111T
WiFi: CC3135 + SIMPLELINK-MSP432-SDK
Bluetooth: CC2564C + CC2564CMSP432BTBLESW1
Sasaki,
Yes the clock frequency is correct. The MSP432P4111T is built for higher temp applications. Because of this, the CPU freq had to be limited to 24Mhz to ensure a stable MCLK throughout the device in higher temp scenarios.