Part Number: MSP432P411V Hello. I have the same problem and Chris answer is great but ¿How can I tell sysconfig I'm using 401V variant instead of 401R? My project properties has 401V variant and consulting the sysconfig configuration at the project's…
Part Number: MSP432P411V Hello,
Does MSP-GANG support Flash writing for MSP432P411V? We think the combination of MSP432P411V, MSP-GANG-432ADPTR and MSP-TS432PZ100 should support MSP432P411V.
Also, does MSP-GANG-SOFTWARE support JTAG/SWD lock and IP Protection…
Part Number: MSP432P411V Hi, My customer is using EEPROM for data storage in the system. They are wondering if MSP432Px internal Flash can be used for such purpose. According to TRM, the Flash memory consists of two banks and programmable with a byte…
Part Number: MSP432P411V Hi,
My customers made a product using MSP430P411V. They want to check the checksum after writing the firmware to the chip. However, we can't access the MSP432P411V.
We also can't access using XDS200 and Uniflash. Therefore…
Part Number: MSP432P411V Hi,
I'm working with the MSP432P411V device and we have made for our customer the solution for programming the flash(address range from 0x0_0 to 0x7_FFFF) and Information memory(address range 0x20_0000 - 0x20_0FFF and 0x20_2000…
Part Number: MSP432P411VT Hello,
Our customer is considering to migrate from MSP432P411V to MSP432P411VT because of the temperature range and want to understand the difference. The main differences look like the blew items.
Temperature range
CPU and peripheral…
Part Number: MSP432P411V
Tool/software: Code Composer Studio
In case of VeREF, it does not respond unless the input is more than 60mV.
MSP-EXP432P4111: VREF2.5V OK, VeREF3.3V OK
MSP-EXP432P401R: VREF2.5V OK, VeREF3.3V OK
Our board (MSP432P411V): VREF2…
Part Number: MSP432P411V Hi,
i am trying to develop a software for SPI communication between the MSP432 and CC2652RB, if there is any reference code, can u please share?
Thank you,
Maniram