Part Number: MSP432P411V
Hello ,
I am using UART driver API's to communicate with my terminal. EVeyrthing works fine unitl I tried to send float data using uart_write API.
Here is my code: uart_resp has the correct data to be sent over uart. But uart_hangs…
Part Number: MSP432P411V hi,
whether can i generate a 1.472 Mhz SPI clock frequency on MSP432 by giving the SMCLK which is configured to 12Mhz as a source?
the SMCLK uses the HFXTCLK with 48 Mhz as a source to produce the 12 Mhz on SMCLK.
if suppose…
Part Number: MSP432P411V Tool/software: Code Composer Studio Hello,
I found the assist tool for functional safety standard including IEC 61508 and ISO 26262. www.ti.com/.../SAFETI_CQKIT
Does this tool support MSP432P411V? Also, is there detail documentation…
Part Number: MSP432P411V Hi,
the requirement is to set the SPI clock frequency to 750Khz, can you please tell me whether my understanding is correct with respective the clock configuration for SPI?
code snippet from the available SDK in MSP432P4111:
…
Part Number: MSP432P411V Tool/software: Code Composer Studio Hi,
I was trying to flash the MSP432P411V based custom board through MSP432P4111 launch pad. While flashing i was getting the following error.
CORTEX_M4_0: Trouble Halting Target CPU: (Error…
Part Number: MSP432P411V
Hi All,
i am working on the DMA using ping pong mode for achieving continuous SPI transfer of 2048 bytes of data, i am able get the code implementations for DMA with ping pong, but i have some queries:
1. how to know that DMA…
Part Number: MSP432P411V Tool/software: Code Composer Studio Hi, Can TI provide us Energy Measurement Software library? This library is MSP432 version of MSP430-ENERGY-MEASUREMENT. www.ti.com/.../MSP430-ENERGY-MEASUREMENT
Thanks and best regards, M.HATTORI…
Part Number: MSP432P411V Tool/software: Code Composer Studio Hi, My customer has questions of IAR/CCS. Which IDE does TI recommend "IAR" or "Code Composer Studio (CSS)"? Does it code size/speed optimization performance between IAR and…
Part Number: MSP432P411V Hi,
I am using MSP432P411 non-rtos project, FATSDRAW project.
C:\ti\simplelink_msp432p4_sdk_3_10_00_08\examples\nortos\MSP_EXP432P401R\drivers\fatsdraw
I modified the setting PowerMSP432_PerfLevel myPerfLevels[]
.activeState …
Part Number: MSP432P411V Tool/software: Code Composer Studio Hi
I have a MSP432P401R (100pin PZ) CCS project which is based on "outofbox_msp432p401r_MSP_EXP432P401R_tirtos_ccs" ( CCS8.0.0 sdk_2_10 )
The project has grown so I am running low…