Hi Ron,
Ok, it sounds like you have it working and moving forward with your project. I'll dig into the details and see if the errata should be expanded.
I will mark this posting as RESOLVED, but if this isn’t the case, please click the "This did NOT…
Part Number: MSP432P411YT Tool/software: Code Composer Studio Hi,
I am looking for MSP432P411Y peripheral driver library.
Where to get MSP432P411Y peripheral driver library?
Please provide support/ web-link ASAP.
Thanks,
Warm Regards,
Nilesh.
Part Number: MSP432P411YT Tool/software: Code Composer Studio Hi,
I have installed CCS v10.1 (latest).
MSP432P401R_classic.h is provided for MSP432P401R.
MSP432P401M_classic.h is provided for MSP432P401M.
But MSP432P411YT_classic.h is not provided under…
Part Number: MSP432P411Y Hi Expert,
Previously, my customer is using MSP432P4111 in their new project and passed their test. However, the price is too high, so they consider to use MSP432P411Y instead. Then they load the same code to MSP432P411Y, but…
Part Number: MSP432P411Y
Tool/software: TI-RTOS
I would like to know if the simplelink SDK RTOS examples for MSP432P4111 works with MSP432P411Y? I realized that single difference related to this IC's is the amount of flash memory available. What I need…
Part Number: MSP432P411Y Hi team,
I wanted to make sure I'm understanding the Nmax_ers spec in the datasheet for MSP432P411Y. Am I correct to say that after 1000 erase and program cycles, it could take 10 times longer to perform flash operations?
…
Part Number: MSP432E411Y We are using the MSP432P411Y with SimpleLink and TI-RTOS for our IoT device. We have produced some prototypes and everything is working fine. But last day I needed the datasheet and could not find it on the TI website. The support…
At a very basic level, you will need to change the header file inclusion. This can be done a number of ways but you want to define one of the following:
/******************************************************************************
* MSP432 devices …
What is a manual reset? Are you cycling power or using the /RST line? The REBOOT RESET command simply calls the following in the BSL.
void BSL432_API_rebootReset()
{
#if defined (__MSP432P401R__) || defined (__MSP432P401M__)
MAP_SysCtl_rebootDevice…