Hello,
Thank you for choosing the TI MSP430F5419 for your project. If you are having issues with I2C, please see the following application note.
http://www.ti.com/lit/slaa734
I cannot comment on to use or configure the MXT640t though as it is not…
Hello YG,
our recommendation would be, in case you want to save as much money as possible, but still have a useful setup, to go in terms of HW with the MSP430 CapTIvate MCU Programmer www.ti.com/.../captivate-pgmr
The CapTIvate Design Center GUI www…
Hi ADITI,
Thanks for using MSP430FR2532.
Are you need the source code for CapTIvate Design Center? ( www.ti.com/.../mspcaptdsnctr ) Sorry that we are not going to provide the source code but you can download the exe file and for reference.
For hardware…
Hello Walter,
seeing the picture of your application, I understand your post in the way, that there will be a certain gap between the casing and the capacitive sensing electrodes on the PCB, as all the components are as well on the top side of the PCB…
Hi Luke,
the CapTIvate module is a quite complex one. It can definitely operate even down to LPM4, if using the VLO. Please consult the CapTivate Technology Guide for further details. You can find this. e.g. going to the CapTIvate Design Center Homepage…
Hi Shreyamsh,
Are you using the latest CapTIvate Design Center (v1.40.00.00)? If not, please upgrade to that.
There was a problem where if there are multiple java installations on your machine the application would not always select the correct one upon…
Hi Sanath,
Our CapTIvate device can support up to 60mm glass overlay.
It is normal that you increase the thickness and the sensitivity will decrease. But we will work with a 4mm glass panel just fine.
We have a GUI to adjust the CapTIvate performance…
Hello Gary,
Good catch on the WDT issue in the CapTIvate example. As Eric mentioned, this was caused by a change in header file that made the header file incompatible with a previously pre-compiled library using an earlier version of the header file. …
Hello Keigo Ishii,
Great question, thank you for posting. We now release the binary image for the HID bridge on the CAPTIVATE-PGMR with the CapTIvate Design Center GUI. We started doing this with the latest version, v1.60.00.00. The documentation around…