Part Number: MSPM0G3507 Hello,
we are using arm-none-eabi-gcc to cross build for MSPM0G3507 MCU. The version set is
arm-none-eabi-gcc: 10.3.1
MSPM0 SDK: 1.20.0.5
If using compiler settings -O0 and -flto code runs as expected.
If using -O1/2/s and -flto…
Part Number: MSPM0G1107 Other Parts Discussed in Thread: MSPM0G3507 , SYSCONFIG , MSPM0G1106 We are trying to build code for MSPM0G1107 in preparation for using that device in the future. We have the following related questions:
When we start with an SDK…
Part Number: MSPM0-SDK Hello,
I was going through the given example of the EEPROM emulation type A, given in the MSPM0-SDK and its related application note.
In the example, the read/ write from/ to the Emulated EEPROM is executed on one data buffer at…
Part Number: MSPM0-SDK Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH ,
Important note for early MSPM0 customers
TI recently launched a new family of Arm Cortex-M0+ MCUs , including the MSPM0L series and MSPM0G series . These MCUs are accompanied…
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: MSPM0G3507 Hi, I am doing FW Test with LP-MSPM0G3507 BD( rev1.0 versions) .
But, PWM is not generating (using mspm0_sdk_1_00_00_04 -> timx_timer_mode_pwm_edge_sleep example)
While browsing the…
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: SYSCONFIG , MSPM0G3507 Hi, MSPM0 Team
I downloaded and installed the latest MSPM0 SDK.
I imported some project and compiled.
But build error is occurred as following.
CCS version : Version: 12…
Part Number: MSPM0-SDK Other Parts Discussed in Thread: LP-MSPM0L1306 Hi,
If I order the LP-MSPM0L1306 from the TI store now, does it come with the latest revision (Production Samples)?
https://www.ti.com/tool/ja-jp/LP-MSPM0L1306
Thanks,
Hi Jim Carlson
Please refer to Migration Guide From MSP430 MCUs to MSPM0 MCUs (Rev. A) on the difference between mspm0 and msp430
Please refer to MSPM0 MCUs Quick Reference Guide (Rev. A) on quick start using SDK and sysconfig
Please use mspm0 SDK https…
Hi Daniel,
The source code and project file with CCS for the DRV8243S-Q1LEVM can be downloaded from the EVM webpage, https://dr-download.ti.com/software-development/support-software/MD-8Fqtr3axho/01.00.00.0B/slvc821b.zip . We do not have a code example for…
Hi Craig,
Are you hoping to prototype the MSPM0 with the BOOSTXL-DRV8323RS? This boosterpack can plug directly into the MSPM0G3507 Launchpad for prototyping. You can find demo code for BLDC motor control in the MSPM0 SDK under \mspm0_sdk_1_30_00_03\examples…