Part Number: TLV758P Other Parts Discussed in Thread: MULTIPKGLDOEVM-823 , Hello,
I test the TLV75801PDBVR on MULTIPKGLDOEVM-823 board. And I use the typical application, set input and output capacitor 0.1uF+1uF+10uF ceramic capacitors, and use R1=11K,…
Part Number: TLV757P Other Parts Discussed in Thread: MULTIPKGLDOEVM-823 Is there recommend maximum value for Cout's ESR on TLV757P?
Or, is ESR_max value not have recommend limit and depend on design condition?
(For example, Vout, transient, accuracy…
Part Number: TLV743P Other Parts Discussed in Thread: MULTIPKGLDOEVM-823 , My customer is looking for an LDO, VIN = 3.3V, VOUT = 2.5V, IMAX = 300mA and the TLV7x3p looks to be a good fit.
Per the datasheet, it looks like the Drop out Voltage @ 2.5V should…
Hi Bart,
The LDO output being higher than its regulation voltage indicates that either a higher voltage rail is leaking onto the LDO output rail or that the LDO itself is damaged. The most telling scopeshot is your last scopeshot where you have isolated…
Part Number: LP2985LV-N Other Parts Discussed in Thread: MULTIPKGLDOEVM-823 , LP2985 Hi Team,
my customer needs to know the minimum load current to operate LP2985AIM5-1.5 stable. The part should be used as a voltage reference.
Thanks
Part Number: TPS763-Q1 Other Parts Discussed in Thread: MULTIPKGLDOEVM-823 Hi team
customer wants Vout = 5.7V at Max Iout 80mA with Vout deviation = +- 3.5%.
he will use TPS76301-Q1 for adjustable Vout.
D/S says Vout deviation = +- 3% for 5V <= Vout…
Part Number: LP3985 Other Parts Discussed in Thread: TINA-TI , , TLV713 , MSP430F2101 , LP3983 , TPS62125 , LP2985 , MULTIPKGLDOEVM-823 , DEM-SOT23LDO Tool/software: TINA-TI or Spice Models Hi,
in order to compare startup behavior of LP3985 (2.5V) to TLV713 …
Hi Abhishek / Aswath,
Do you still have the multimeter connected when you took the second measurement? It would be normal to have a drop on the order of 15mV as you scale the load to 250mA, but 200mV seems really high. Are you testing the LDO on an EVM…