Part Number: NE5532 Hi TI,
I have a simple question. We bought some NE5532DR chips on digikey. The chips are labeled with N5532. I had some NE5532 chips in my storage which I used for our circuit. My problem is that the new chips N5532 behave different…
Part Number: NE5532 Other Parts Discussed in Thread: OPA210 Hi team,
My customer met a problem using NE5532P, here is the schematic and waveform about the output.
You can see the output has ripple. Do you have any good advice?
Part Number: NE5532 Other Parts Discussed in Thread: OPA2134 Our customers used ne5532 model and sop8 package before. Now they can't purchase it. Please which model can be used to replace it directly? The product is audio power amplifier.
Part Number: NE5532 Dear Team,
my customer using NE5332 for their product.
The Vcc-Max can reach 22V in the datasheet,
but I see that the recommended Vcc is up to 15V We have a product Vcc that will use 19V DC, does any concern to use the 19Vdc…
Part Number: NE5532 Other Parts Discussed in Thread: RC4558 Hi team ,
We can see that there is a super balanced circuit built with ne5532 in professional audio equipment.
It is said that this circuit can keep the impedance of the two input ports…
Part Number: NE5532 Hi, I setup a simple 12x inverting op amp, feeding it 100mV P-P such that the signal never hits bellow ground (0V). Text book example. The circuit doesn't work. But if I supply +/- 5V the IC works as expected. As an Op Amp or Comparator…
Part Number: NE5532 Hi Team,
Could you please let us know the actual max value of Equivalent input noise voltage (Vn) of NE5532(Null version)?
<Background>
I understand that NE5532A(A version) guarantees max value of Vn but I can’t get NE5532A…
Part Number: NE5532 Other Parts Discussed in Thread: LM386 , TPA3138D2 Hi Team,
NE5532 audio amplifier, the application of loudspeaker 8Ω single-ended amplification. Output wave distort when carrie the Load,while not carrie the load, the wave is ok…
Part Number: NE5532 Hi Team,
We would like to decrease the equivalent input noise voltage of NE5532.
Generally, if JFET is set to the input of bipolar amp, this amp can decrease equivalent input noise voltage.
Could you please let us know if you…