This is the da850-lcdk.dts file
/* * Copyright (c) 2016 BayLibre, Inc. * * Licensed under GPLv2. */ /dts-v1/; #include "da850.dtsi" #include <dt-bindings/gpio/gpio.h> #include <dt-bindings/input/input.h> / { model = "DA850/AM1808/OMAP…
Other Parts Discussed in Thread: OMAP-L132 , ADS802 , OMAPL138 , OMAP-L138 Hi,
My customer would like to know if OMAP-L132 support a direct connection to the ADS802?
Thanks
Marcus
Other Parts Discussed in Thread: OMAPL138 Hi,
I want to use the MCBSP1 RBFIFO with EDMA for data receiving on OMAP L132. As described in the reference manual, the EDMA source address is set to the RBUF address of the MCBSP RBFIFO, that is 0x01F11000. And…
Hi Anurag,
Please refer to application note Using the OMAP-L132/L138 Bootloader for instructions. In addition, OMAP-L13x/C674x Resources and FAQ can be very helpful as well.
Regards,
Jianzhong
Hi Ben,
Processor-SDK for TI RTOS only supports MMCSD SBL as documented here . It doesn't have support for NAND flashing.
You can still use the omap-l138 starterware which has NAND SBL . However, we don't support the starterware anymore. You can refer…
Hi Mark, There's some note on how to apply the workaround for "Advisory 2.3.24 Boot: ECC Data Error in Spare Area Causes NAND Boot Failure" in OMAPL138 Errata >>> The software patch is available as a pre-built file with the latest…
Other Parts Discussed in Thread: OMAP-L132 , OMAP-L138 , OMAPL138 Hi:
I am looking for resources for the OMAP-L132 and I haven't found much! Most of the available support is for the OMAP-L138. Could someone please direct me to the L132 resources? Also,…
Part Number: OMAP-L138 Other Parts Discussed in Thread: OMAPL138 , OMAP-L132 Hello guys,
Currently, I am working on a secondary bootloader for my OMAPL138. I think that it would be a good start, if I can get TI bootrom and add some extra functionality according…
Other Parts Discussed in Thread: OMAP-L132 , ADS5520 , OMAP-L138 , DM3725 , DM3730 The OMAP-l132 says that the maximum DSP speed is 200MHz. What does this mean exactly? I'd like to use an ADS5520 running at 125MSPS with the OMAP-l132. Is this feasible or not…