Part Number: OMAP-L138 Good Day,
I am having a problem writing the flash of a Omap-L138 custom board. I have a back up .bin that I would like to write to the nor flash to repair a firmware flash error that resulted in a non functional unit. I have been…
Part Number: OMAP-L138 Hello,
It was developed using CCS5 before, but it is no longer compatible with win10. What version of CCS should I use? Are there any relevant environmental guidelines?
Regards,
Gary
Part Number: OMAP-L138 Dear all,
As SFH utility is used to burn the images to OMAP-L138 microprocessor, so we required its source code so that we can change to serve our purpose.
We tried but could not found on internet. Please provide the source code…
Part Number: OMAP-L138 hi.
I am using omap-l138.
I have a question about using usb0 interface. The usb0 interface is used as a device.
USB operates well even if 5V power is not supplied to the USB0_VBUS pin.
Is it okay to not supply 5V to the USB0_VBUS…
Part Number: OMAP-L138 I bought the component OMAPL138EZWTA3E by mistake instead of OMAPL138EZWTA3. The E refers to a security feature.
Can I use OMAPL138EZWTA3E like OMAPL138EZWTA3 without additional hardware?
If there is no solution, what hardware…
Part Number: OMAP-L138 Other Parts Discussed in Thread: OMAPL138 Hello Champs, Customer can program flash on OMAPL138EZWTA3, but it can't program flash when using OMAPL138EZWTA3E secure version. It prompted below error. Thanks Regards Shine
Part Number: OMAP-L138 UART RX always has data, DSP starts,UART can't enter the interrupt. if DSP starts first, RX on UART normally enters the interrupt to receive data.
Part Number: OMAP-L138 Hello Champs, Customer wanted to print 6 fractional floating point.
float a = 1.234567;
System_printf("%f\n", a);
System_printf("%.6f\n", a);
But the result is 1.2345 Is there some special to configure? Thanks R…
Part Number: OMAP-L138 Hi team
Can you help to check does those two DDR can fulfill OMAP-L138 DDR needs, since there is the supply issue in customer's original design, they want to double confirm with us on design change.
W971GG6NB_A01.pdf M14D1G1664A…