Other Parts Discussed in Thread: 10G-EXPANSION-EVM Hi
I have the Part number but it is not recognise... Part Number is 10G-EXPANSION-EVM
Please can you provide the CE/EU Declaration of Conformity for 10G-EXPANSION-EVM ?
We, Mouser USA, have this product…
Part Number: TPS65987EVM Hello,
I have to design an interface between a PC that supports Thunderbolt and a system. One video signal and one audio signal are sent to the system from the PC, and there is a USB2 communication between both too (please see…
Part Number: ONET-10G-EVM Hello Sir,
We want to using a SFP+ EVB to test our SFP+ module ( xsgpon and 10GBASE-LR). Can ONET-10G-EVM meet our requirement?
There are instructions on the TI web that this product also comes with a SFP+ module, can yout provide…
Part Number: ONET-10G-EVM
Will this evaluation board be able to drive an 850nm vcsel? Would we require impedance matching anywhere?
Can we drive this board using a function generator?
Are we able to solder the wires at the output that directly feeds…
Part Number: ONET-10G-EVM Hi,
I 've got a ONET-10G-EVM kit but there is no user manual and the GUI is locking into initialization window. The email ling for the manual is not working as well. Why is it so a big secret? Should it be available online…
Part Number: ONET-10G-EVM Tool/software: TINA-TI or Spice Models The link http://www.ti.com.cn/tool/cn/onet-10g-evm?keyMatch=onet-10G-EVM&tisearch=Search-CN-Everything
There is no shematic and user guide in this link . Would you please provide the…
Part Number: ONET-10G-EVM Hi,
I see from the previous thread that the ROSA used in the ONET-10G-EVM is SRO2-10F-LC-T-I . And the TOSA is TX293k. Could somebody explain that why the ROSA is at 850nm while the TOSA at 1310nm?
Thanks
Zhao