Part Number: ONET4201PA Other Parts Discussed in Thread: ONET4201LD Are there IBIS or *** models available for the following devices?
TI - ONET4201PA (limiting amp.)
TI - ONET4201LD (laser driver )
Hi Lillian,
For the MAX40659, we recommend the LMH32401 as our closest alternative. For the MAX3748, we recommend the ONET4201PA.
Best Regards,
Ignacio
Part Number: ONET4201PA I have a design the uses several of the ONET4201PA limiting amplifiers. I am looking at the eye diagrams of the copper side of the amplifier. One one channel, the eye diagram looks reasonable. On others, the eye looks terrible…
Part Number: ONET4251PA Other Parts Discussed in Thread: ONET4201PA Hello Team,
is there info available about the bandwidth of the RSSI circuit of ONET4251PA & ONET4201PA. I need to monitor changes in the range of several kHz.
Thanks in advance. …
Part Number: ONET4201PA Hello,
In 4Q16, we were told that the ONET4201PYS bare die would be available
In 1Q17. We tested the packaged part and demonstrated excellent performance
With the packaged part. We designed the ONET4201PYS bare die into a cri…
Part Number: ONET4201PA Hello Team,
I have a customer who is working with the ONET4201PA and is unsure why the Max junction temperature is rated more then the storage temperature.
" The max junction temp is +125°C which seems to conflict with the max storage…
Other Parts Discussed in Thread: ONET4201PA Dear Sir:
I used ONET4201PA and have a issue that is test failure at optical +0dBm eye diagram.
Is that ONET4201PA spec can't meet 0dBm eye diagram test?
Compentitor is MNDSPEED M02050 which can pass 0dBm…
Other Parts Discussed in Thread: ONET4201PA The onet4201pa datasheet lists the LOS pin as a CMOS output but with a low hi level drive capability (30 uA)
Is it possible to overdrive (force a ground in a wired OR fashion) without affecting the output driver…
Other Parts Discussed in Thread: ONET4201PA Here are the questions for the ONET4201PA;
- what is the propagation delay through the amp (I could not locate this in the datasheet). - they would also like to use this as single-ended input, AC coupled. Will…