Part Number: ONET1151P Tool/software: Hi,
can I connect these two drivers with 2 wires of I2C (SCK and SDA) in cascade connection? each driver gets different address
do you have any layout recommendation for this connection?
Part Number: ONET8501V Other Parts Discussed in Thread: ONET1151P , Dear Team,
For a thermal analysis my customer is asking for thermal resistance, maximum case temperature and T junction for components ONET8501V, ONET1151P.
We've noticed it doesn't appear…
Part Number: ONET8501V Other Parts Discussed in Thread: ONET4291VA , Hello TI!
I am in the process of replacing, in my electronics, the laser driver ONET4291VA because it is turning obsolete (LTB).
At the moment I am thinking to use ONET8501V. Can you say…
Part Number: ONET8501V Other Parts Discussed in Thread: ONET8501P Hello,
My customer is looking for an alternative solution for the DS1878.
Is there a way or device to replace DS1878 functions when using ONET8501V and/or ONET8501P?
Thank you.
JH
Part Number: ONET8501V The data sheet says [date rates from 2Gbps up to 11.3Gbps], Is it possible to use at 1Gbps? Please let me know if you have any problems or risks.
Part Number: ONET8501V If there is no load connected to the MOD+/MOD- terminals, or if a high impedance load is connected to the MOD+/MOD- terminals and the maximum output voltage level (IMod=24mA) is set, is there any problem or danger?
For example,…
Part Number: ONET8501V Hi
I'm trying to use the ONET8501V, The datasheet and the design are for 2007. I was wondering if there is another update or a new version available. would you please let me know?
Regards
Moein
Part Number: ONET8501V Other Parts Discussed in Thread: TIDA-00088 Hello,
I am reading following document.
There seems to be a projejct that runs on MSP430 for SFP+ module.
And I think it is also the firmware for TIDA-00088.
Is it available?
I would like…
Part Number: ONET8501V Hi Experts,
Our customer wants to know if the Laser Safety features are still active in open loop mode for ONET8501V, can you help to check? Thanks a lot!