Other Parts Discussed in Thread: OPA4134 Hi everyone!
So for some reason I need to add an offset of 3.6 V to a sinusoidal signal. I have set up a circuit according to this schematic:
I know that there are probably easier ways to do this but it should…
Other Parts Discussed in Thread: OPA134 , OPA1641 , OPA827 I want to use an OPA134 connected as a unity gain follower with a fixed load of 1kohms.
Then I want to take the signal out of the supply rails via cascodes and mirrors so that I can get an…
Other Parts Discussed in Thread: OPA134 Hello .
There is a project which I am working on in our University which needs me to simulate the OPA134 model in Mentor Graphics Hyperlynx Software .
OPA134 Spice model is available but please provide me…
Hello .
There is a project which I am working on in our University which needs me to simulate the OPA134 model in Mentor Graphics Hyperlynx Software .
OPA134 Spice model is available but please provide me with the model for OPA134 which can be used…
Part Number: OPA132 Other Parts Discussed in Thread: OPA134 Tool/software: HI, staff
In Rev.C, the Trim terminal has been removed and changed to an NC terminal, so I would like to check the terminal processing method.
OPA132 データシート(SBOS0504C) The…
Part Number: NE5534A Other Parts Discussed in Thread: NE5534 , SA5534 , OPA134 The NE5534AP is listed as LTB.
There is a new part on the 5534 page: NE4434APE4.
But all links for this part appear to be broken.
Is this part available & is there…
Part Number: OPA627 Other Parts Discussed in Thread: OPA134 , OPA140 , OPA145 , LM124
Tool/software:
Hello,
I work on legacy avionics systems made by J.E.T. These originally used Burr Brown 2A180 / Analog Devices AD3417 precision op amps, which…
Part Number: NE5532A Other Parts Discussed in Thread: NE5534A , OPA1677 , OPA134 Hello,
According to sales team's information, NE5532A/NE5534A include G4 and E4 devices are going to EOL caused by FAB matter.
Could you suggest us TI replacement device…
Part Number: OPA328 Other Parts Discussed in Thread: OPA134 I was looking for a newer part to illustrate some SSBW vs Gain issues, the OPA328 Aol phase, if I add that 20pF load, looks about right,
However, if I remove that 20pF (as would be a normal…
Part Number: THS3217EVM Other Parts Discussed in Thread: OPA134 Hello
We are new to this board and are not sure of having read the manual properly. The issue is we get 4 mV or 40 mV when we use the OPS amplification even if the differential signal we…