Part Number: OPA1633 Other Parts Discussed in Thread: OPA1637 Hi Expert,
Customer looking for audio AMP solution to achieve differential signal input to single-end output. do you have recommend solution for this?
Regards,
Mark
Part Number: THS2630 Other Parts Discussed in Thread: OPA1633 , OPA1632
I am looking for a single-ended to differential ADC driver.
The input is a single-ended signal span between -12 V & +12 V, frequency up to 25 MHz. I need to convert the +/-12 V…
Part Number: TAS6584-Q1 Other Parts Discussed in Thread: TAS5634 , TAS5548 , OPA1633 Tool/software: I would like to design Class H Audio Amplifier solution of 10 CH with two TAS6584-Q1 and LM5123 Boost Controller which will work the audio power supply…
Hello Supira Medical,
Okay, I will send over my thoughts once I have them. We also have OPA1633 as a newer device with upgraded performance.
Best,
Alec
Hello Shreeprada,
I have an EVM and I will be testing the OPA1633 tomorrow for other support. I can use the same EVM to also test the OPA1632 tomorrow or Friday.
Best,
Alec
Hello Max,
You can download the BUF634A spice model from the TI product page and use in TINA-TI. Typically the models on the TI website are more up-to-date than the models internal to TINA-TI, which could also explain some simulation issues.
I am looking…
Other Parts Discussed in Thread: OPA1633 , OPA323 , TAC5112 , PCMD3140 , PCMD3180 We are making a stethoscope using MEMs digital Mic with 20hz to 20Khz and wish to use TI Preamp and Op Amp and are thinking to use OPA323 as Preamp and OPA1633 as amplifier for…
Part Number: ADS1174 Other Parts Discussed in Thread: OPA1632 , OPA1633 , OPA350 , REF3325 , OPA2350 Hi,
I have attached my current schematic for an ADS1174 circuit (based on the datasheet implementations) to acquire a single ended input signal with 0-2.9V…
Hi, Jeff
Actually i want to convert differential input signal to single-ended signal something like below:
But when i do it with LM386 i think i got gruond loop. i got echo when i make a phone call and talking. I found this one
https://e2e.ti.com/support…
Part Number: OPA1612 Other Parts Discussed in Thread: PCM1794A Hello Mr or Mrs.
Happy new year~!I am always grateful for your help. :)
I am designing a circuit which is related DAC output and it confuses me.
This is a PCM1794a reference TINA simulation…