Part Number: OPA192 Other Parts Discussed in Thread: LM2664 , LM7705 , TLV387 Tool/software: Hi.
I have a problem with the OPA192.
OPA192 is used as a low impedance buffer to the input of the MCP2024 ADC.
From time to time, all of a sudden the OPA192 is…
Part Number: OPA192 Hi ,
I like the fact that the OPA192 has built in RF/EMI rejection and need that in my application.
I would like the PSPICE model for the OPA192.
Ken
Part Number: OPA192 Hello,
I am looking to use the OPAH014-SEP as a current sense amp as shown in the picture below. I am looking to use it to measure the current from power supplies (2V, 2.2V, and 3.7V). The preferred power supply rail I want to used…
Part Number: OPA192 Hi Team,
My customer, KLA, has a couple of questions about the OPA192 Op Amp.
When simulating our circuit it shows that this Op Amp has problems converging with un-balanced supplies.
(We were thinking of operating with -5V and +24V…
Part Number: OPA192 Hi Team,
In my customer's case, OPA192 is configured as high side current sensing circuit, and the Vs+ is coming from the upstream Flyback converter aux winding. The aux winding is unregulated, so Vs+ will shift between 18V and 21V…
Part Number: OPA192 Hi Expert,
My customer mentioned that OPA192 has output signal delay issue as pic.
Please share some comment and recommendation for us. Thanks!
Part Number: OPA192 Other Parts Discussed in Thread: XTR111 ,
I am designing an iepe signal conditioner and as seen in the introduction I have a 2nd order butterworth high pass filter.. When the sensor (load) is not connected, the current source with 24…
Part Number: OPA192 Other Parts Discussed in Thread: OPA2192 , INA296A Hi,
I am using an op-amp configuration as shown in the attached image for converting 0.01V pk-pk sine waveform (ac output current of the inverter, around 100A pk-pk, derived from the…
Part Number: OPA192 I hope to know which resistance value listed in P. 6, P. 9, P11 is the output resistance of this OPA192 device? Or none of these 3 resistance values is the output resistance value of this device and the output resistance of this is…