Part Number: OPA192-Q1 Hello OPAMP team,
I'm Gilberto.
I have two questions.
1. which is the Overvoltage protection value when the power is off?.
2.which is the Input Impedance value when the power is off?
Thanks,
Gilberto DIAZ
Part Number: OPA192 Other Parts Discussed in Thread: TINA-TI Hi guys, I would like to use the OPA192 as a comparator in my application. However, in TINA-TI, I keep getting convergence problems with the simulation attached to this post. Can you please comment…
Part Number: OPA2192 Other Parts Discussed in Thread: OPA192 Tool/software: Hi team,
I use below circuit to test the CMRR of OPA2192:
however the result is different from datasheet:
datasheet shows opa2192`s CMRR can keep 140dB till 10kHz, but my test…
Part Number: OPA192 Other Parts Discussed in Thread: TINA-TI ,
Hi,
I would like to simulate the stability with each temperature on TINA-TI.
Simulating the stability, I need inputting the equivalent to calculate loop gain as below.
However, the error…
Part Number: OPA192 Other Parts Discussed in Thread: OPA862
If my input is grater than VCC will the show leakage to the VCC
eg: V+=5V and V-=0V and ,my input is 32V . will this 32V show leakage to my V+ pins. Which i meant is will my V+ voltage will have…
Part Number: OPA192 Hi Shadders,
I think you have short-circuited R3 somewhow when experimenting with the circuit. This would not only explain the damaged OPA192 but also the damaged zener diode.
By the way, I don't understand, why you have mounted back…
Conor,
There are two important things to consider when protecting op amps with input steering diodes like the OPA192.
You must limit the maximum input current to 10mA or less. Typically I try to limit the current to 1mA for a safety margin. The way…
Part Number: OPA828 Other Parts Discussed in Thread: OPA192 , Tool/software: Hello team,
My customer is evaluating OPA828. The electrostatic discharge of OP828 is ±2000V. But some opamp (ex OPA192) cases are ±4000V.
Is this due to the difference…
Part Number: OPA192 Hi Colleague,
In our customer current scenario, there will be a 14V in OPA192 output in some special time.
So the customer wants to confirm:
1. Whether OPA192 will be damaged?
2. If OPA192 will be damaged, how to add a protection circuit…
Part Number: OPA192 Other Parts Discussed in Thread: TVS1400 Hi Colleague,
In our customer current scenario, there will be a 14V in OPA192 output in some special time.
So the customer wants to confirm:
1. Whether OPA192 will be damaged?
2. If OPA192 will…