Part Number: OPA197 I am working with a OPA197QDGKRQ1 and am seeing good results with 1MOhm resistors in Tina TI. Are there restrictions for high impedance with the OPA197?
Part Number: OPA197 Dear Thomas-san,
Thank you for your response. I understand the contents.
However, which item in the data sheet can be understood that Vo1 and Vo2 output is clipped at about 5.77V and 230mV?
Best regards.
Part Number: OPA2197 Other Parts Discussed in Thread: OPA197 , LF353 I'm using the OPA2197 dual opamp in an inverting opamp summing junction with 3 input signals. The device is powered from +/-12Vdc. Each input signal consists of an 25Khz to 60Khz 2Vpp…
Part Number: OPA197 The OPA197 datasheet shows two propagation delay figures (Figure 39 and 40).
Is this real or an error in the datasheet? The delay times shown seem not to match the speed performance of the part.
BR
Wulf
Part Number: OPA197 Hi Team, Our customer is requesting for the continues power consumption details of the following op-amps:
1. OPA197IDBVR 2. OPA365AIDBVR 3. TLV2313IDGKR If it is needed to create separate threads for these devices, please let me know so…
Part Number: OPA197 Hello team,
OPA197 integrates EMI filter inside the device and can reduce EMI effect from the source.
However, I think we still see the effect(offset shift on output) even with device integrating EMI filter such like OPA197.
In the…
Part Number: TLE2037A-Q1 Other Parts Discussed in Thread: TLV197-Q1 , OPA197-Q1 , OPA192-Q1 , TLE2141-Q1 , OPA1612-Q1 Hello,
Good day, Customer wants a TLE2037a-Q1 pin to pin device within 1Mhz. Could you please give a recommandation. Thank you.
Part Number: OPA197 Hi Amp forum team,
I am an engineer who want to make an analog buffer circuit with OPA197.
In order to identify an input impedance of OPA197, I saw below char on datasheet.
I have two question about above chart.
1. What is the…
Part Number: OPA197 Dear Team,
OPA197 is used in a circuit where during failure condition an undervoltage situation can happen. In this case the supply voltage collapses to about two volts. It can be observed that the Iq which is normally in the 1mA…
Part Number: OPA197 Hello,
OPA197 datasheet only appears to specify input offset voltage (Vos) at 25deg.C.
Please advise Vos spec. between 0deg.C to 85deg.C as well as at -20deg.C for operation at Vs = +/-18V across the entire common mode voltage range…