Part Number: OPA2171 Other Parts Discussed in Thread: OPA4171 , , OPA4991 , OPA2991 , OPA2990 , OPA171 Hi Team,
We have received this inquiry from our customer,
I have been using this opamp as well as opa2171 and opa4171 as it was advised by a member of your…
Part Number: OPA2171 Other Parts Discussed in Thread: OPA2991 Hi team,
Could you please help us review below customer's OPA2171 circuit schematic? The high value of resistors provide isolation function here.
Best Regards,
Stanley Dai
Part Number: OPA2171-Q1 Other Parts Discussed in Thread: OPA2171 Hi Experts,
For below output voltage swing range of OPA2171-Q1, is it guaranteed in whole life time under -40-125C temperature range? Due to the aging of the components, will it cause additional…
Part Number: OPA2171 Hi TI,
As shown below, the data sheet shows the maximum voltage rating of the signal input.
When the supply voltage is 5V and the input voltage (V+) is 10V. Does that mean the IC could be damaged?
Part Number: OPA2171 Other Parts Discussed in Thread: TLV9002 , TLV9062 , OPA2990 Hi team,
When I read the OPA2171 datasheet, there are different descriptions about the power supply range.
1. Features:
2. Recommended ranges:
So my custoemr wants to…
Part Number: OPA2171 hi dear supporting team,
double check with you, for single supply application, customer get -0.82V at OPA2171 Vin+ input which has exceed the absolute rating, 2.3mA input current which still smaller than 10mA limitation, will it cause…
Part Number: TLV9352 Other Parts Discussed in Thread: OPA2171 , , OPA171 , OPA172 Hi team,
My customer used OPA2171 and the SCH put in below Pic1. The cap C403, C203, C218, C209 have been removed in the board.
J13 interface is the "input" and U_OUT_ADC0…
Part Number: OPA2171 Dear Team,
Can I connect V+ to ground and V- to 12V for sensing the negative input signal?
I think the answer is yes, right?
BR
Kevin