Part Number: OPA2210 Hi
I would like to know whether the die used in single, dual and quad packages is the same or is a different die. Also are these parts packaged at the same location or at different locations?
TI
OPA2210ID
SOIC-8
Dual -…
Part Number: OPA2210 Other Parts Discussed in Thread: OPA2333-HT , OPA211-HT , OPA2211-HT Hi Team,
Is there TI solution to replace ADI AD8634HRZN? AD8634HRZN temperature is -40C to 175C, however OPA2210IDR only up to 125C.
Please suggest. Thanks.
Part Number: OPA2210 Other Parts Discussed in Thread: OPA2211A , OPA2828 , OPA2189 Hi TI,
I am looking at an application, in which OPA2210 can meet almost all requirements, except its slew rate. Do you have any part suggestions? I need ~3x OPA2210 slew…
Part Number: OPA2210 I am trying to use OPA2210 as a front-end differential buffer, and from the datasheet, the maximum drift is 0.5uV/K. Considering these are not matched op amps, how should I consider the total offset drift? I am thinking for the worst…
Part Number: OPA2210 Other Parts Discussed in Thread: OPA210
Hi,
I need to simulate the stability for OPA2210. I download the TINA model from TI website. And I have done a TINA simulation. But I am not sure CF and RISO value is correct.
OPA2210 input…
Part Number: OPA2210
Hi,
I need to simulate the stability for OPA2210. I download the TINA model from TI website. And I have done a TINA simulation.
According TI VIDEO, find the frequency value when Aol=20db. So f is 269khz when Aol=20db.
Then RISO=1…
Part Number: OPA2210 Hi team,
The OPA2210 Exposed Thermal Pad, where should I connect it to?
Can I connect it to the solid pattern of floating potential?
Regards,
Masakazu
Part Number: OPA2210 Other Parts Discussed in Thread: OPA1656 , OPA1622 , OPA1662 , BUF634 Hello,
Referreing to fig. 6-6 in the OPA2210 Datasheet SBOS924G , it seems rather strange that the THD+N is less in the non-inverting configuration, when both inputs…