Other Parts Discussed in Thread: OPA2348 Our customer will use epoxy for waterproofing for their application. When the OPA2348 covered by epoxy, does the OPA2348 work nomally?
Device : OPA2348AIDCNR Epoxide manufacturer : Three Bond Base compound : 2001 Curing…
Other Parts Discussed in Thread: OPA2348 Hi all,
I hereby included the schematics of my instrumentation op amp design by using OPA2348 with a gain of 21(By using the formula of G=(1+2R1/Rg)R3/R2). In my design R3=R2=10K and R1=10K and Rg=1K. I gave a…
Other Parts Discussed in Thread: OPA2348 , UA741 , OPA348 Hi all,
I am using OPA2348 to amplify my differential signal by implementing a instrumentation amplifier.But it is not working for me.When i am implementing the same circuit with UA741,I can able…
Other Parts Discussed in Thread: OPA2348 I have prototyped up the attached circuit using the OPA2348 and am wondering if you can help me understand the results I am getting.
Conditions:
CONN_PIN is unconnected
SEL0 = 0V
SEL1 = 0V
SEL2 = 5V
SEL3…
Other Parts Discussed in Thread: OPA2348-Q1 , OPA2348
There appears to be an automotive qualified version of OPA2348 (OPA2348-Q1), but only in the 8-SOIC package. For space, I would like to use the SOT23-8 version of the non-qualified device. Can you…
Other Parts Discussed in Thread: OPA2348-Q1 , OPA2348 TI Team,
There appears to be an automotive qualified version of OPA2348 (OPA2348-Q1), but only in the 8-SOIC package. For space, I would like to use the SOT23-8 version of the non-qualified device. …
Part Number: TIDA-01513 Other Parts Discussed in Thread: ISO7741 , ISO7710 , ISO7741-Q1 , ISO7761 , ISOW7841 , ADS1118 , , OPA2348 Hi Team
I would like to use the insulation leak measurement circuit insulated from a 1000V battery.
1. We believe that the circuit…
Part Number: OPA2347 Other Parts Discussed in Thread: OPA2348 , OPA2313 , TLV2333 Hi,
What is the ESD class and voltage rating of ESD protection of the pins on this device?
Thank you,
HSG
Part Number: OPA4322-Q1 Other Parts Discussed in Thread: OPA2348-Q1 , Hello TI Team,
I am using both of the above op amps (OPA4322-Q1 and OPA2348-Q1). When these op-amps are off ( It is possible that (+) input voltage can go up to 16V through a 49.9k resistor…
Part Number: OPA348-Q1 Other Parts Discussed in Thread: OPA4348-Q1 , , OPA2348-Q1 , OPA2348 , OPA4348 , OPA348 , TLV3701 , TLV3702 , TLV3704 Hi Team
my Customer has the following questions about FIT for OPA348-Q1/OPA2348-Q1/OPA4348-Q1.
may I expect your swift…