The electrical parameter can refer to the OPA2365 and comes with butterworth filter features. The application is for the motor Encoder Endat2.2/1387 for Sine & Cosine signal transfer.
Part Number: OPA365 Other Parts Discussed in Thread: OPA2365 , OPA615 Hi all Would you mind if we ask OPA365? Our customer is looking for following a substitute(Sample and Hold circuit device). https://www.intersil.com/content/dam/Intersil/documents/ha53…
Hello Sognzhen,
MTBF/FIT estimates can be found in the link Kai shared. For Pin FMA, the OPA607-Q1 will be very similar to these examples: OPA858-Q1 and OPA2365-Q1 . Our high speed amplifiers tend to be on the straightforward end on pin failure modes…
Hi Devin,
The opamp is OPA2365.
I switched our control card to the TI control card (TMDSCNCD28377D_180cCARD_pinout_R1_3) and rewired the signal. Since the TI card has no installed resistance, the voltage did not drop that much: 1.455 V from 1.502…
Part Number: TIDA-00202 Other Parts Discussed in Thread: OPA2171 , OPA2365 , OPA171 , OPA365 Customer is modifying the TIDA-00202's circuitry of the SINE and CONE Signal conditioning for hyperface requirement.
There are some R, C and OPA changed(Removed…
Hi Michael,
Here is an E2E that discusses non-magnetic https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/965672/opa2365-for-mri-applications
and asks this question:
. . . open to using unpackaged/bare die devices ? That way…
Other Parts Discussed in Thread: ADS7263 , OPA2365 Dears,
In the datasheet, ADS7263's application circuit is used the OPA2365. Is it specify use theOPA2365 or the OPA what need satisfies performance requirement?
If the input signal is ±10V, I want…
Part Number: ISOW7842 Other Parts Discussed in Thread: CC2538 , CC2592 , OPA2365 , Tool/software: WEBENCH® Design Tools Hello TI, I am working with ISOW7842 to isolate CC2538 & CC2592 board with Microwave sensor amplifier OPA2365 to avoid the interference…
Hi JD,
Inductance shouldn't have any effect on charge times unless you want to include resonance calculations. The TI OPA2365 has a bandwidth of 50MHz. At least as far as speed is concerned, you would be limited by the ADC not the OPA2365.
Hi jars121,
Nice, that is a more compacted layout!
jars121 said: I'm using a 4 layer stack (signal, GND, PWR, signal); do I need to use stitching capacitors if I put these components on the bottom side?
If you have ground plane fills on the top…