Other Parts Discussed in Thread: OPA2670 , OPA2673 , THS6212 , THS3202 , THS3201 Hi,
Can anyone please provide the OPA2670 Tina spice model. It will be very helpful for simulation.
Thanks and Regards,
Lokesh E
Part Number: OPA2675 Other Parts Discussed in Thread: OPA2670 , STRIKE , OPA2677 Hello E2E Experts,
Good day.
I am developing a laser communication system. For the laser transmitter, we have split the project into the laser bias controller and the laser…
Kai is correct, the AFE031 is for the very low speed (metering kind of thing) Cenelec while THS6222 is the line interface driver for the much high speed PLC apps on grid powerlines. There in house PLC drivers and applications as well that are again different…
Part Number: THS6212 Other Parts Discussed in Thread: OPA2673 , OPA2670 , THS6222 , THS6226 , THS6214 Dear Sir:
I am searching for a suitable VDSL line driver.
TI THS6212/621 4, OPA2673, OPA2670 seems all can support VDSL2.
Pls can you teach me where I can…
Part Number: OPA2673 Other Parts Discussed in Thread: OPA2677 , OPA2670 , THS6301 To whom it may concern,
I wonder if the two 1/2 amplifiers in OPA2673 are designed only to operate in a differential fashion, or can I just use 1 of the 2 amplifiers, with…
Hi Jose,
Few options to consider for your application would be THS6132, THS6182, THS6002, THS6012, OPA2670. There are quite a lot of options which you can also browse through in TI High Speed Amplifiers http://www.ti.com/lsds/ti/amplifiers-linear/high-speed…
David, Neil,
The OPA2670 uses a fully differential architecture and cannot be used as two individual op amps. The OPA2673 is a very similar part but is not fully-differential meaning that the 2 op amps can be used separately. There is a Spice model for…