Part Number: OPA2990 Hello TI
I would like to use an OPA2990SIDGSR (or maybe different housing type) in a circuit and therefor I would like to know, if it is possible to apply voltages of up to 30V to the OpAmps output pin, when the output ist shut down…
Part Number: OPA2990
Hi Team
My customer is try to make a S/H circuit using the OPA2990, and they want to know whether the open-loop or the close-loop is better for this application considering the accuracy.
Also, is the follower output or the integrator…
Part Number: OPA2990 Hello. I have a question about the absolute maximum rating of the supply voltage of the OPA2990IPWR. It is stated that the minimum supply voltage is 0 [V] in the data sheet. However, when I measured the voltage before the power was turned…
Part Number: OPA2990
Folks,
I'm writing to confirm the SHDN functionality and thresholds. I believe that the SHDN function works like so:
SHDN
Logic LOW = (V-) to (V-) + 0.2V = Amplifier enabled
Logic HIGH = (V-) + 1.1V to (V-) + 20V= Amplifier…
Part Number: OPA2990 Hi support team.
My customer would like to know when is RTM for DGK package(VDSSOP-8).
Please let me know if you could provide the information about it.
Best regards,
Higa
Part Number: OPA2990 Hello,
My customer would like to know Vout headroom and footroom vs Iout. Could you provide the plots, Vout vs Iout, like the following, please?
Best regards, K.Hirano
Part Number: OPA2990 Other Parts Discussed in Thread: TINA-TI hello,
I have query regarding SBOA347 DOCUMENT ( www.ti.com/.../sboa347.pdf ). We have to sense high side current. In that main query is supply which is negative, in my application VBUS is…
Part Number: OPA2990 Hi Team,
I would like to use OPA2990S the following powerup sequence.
1. V- = -15V (VS= -15V)
2. V+ = +15V (VS=30V)
According to datasheet, absolute Maximum Ratings of “VS = (V+) – (V–)” is 0V to 42V.
Can…
Part Number: OPA2990 Hi Engineer from TI,
I have a more specific question regarding the OPA2990 operational amplifier and its EMC protection. We test EMC according to DIN EN 61326-1. We currently see no problem with ESD. At burst 1kV the operational…
Part Number: OPA2990 Hi Team,
Could you please let us know RTM of OPA2990SIDGSR (VSSOP PKG)?
Our customer would like to use VSSOP PKG.
Regards,
Kanemaru