Jonathan,
Chopper amplifiers are an excellent choice for low offset, and low offset drift. However, the chopping calibration process generates current transients on the inputs of the amplifier that translate into input offset when large feedback and input…
Hi Tim,
As you correctly diagnosed, the LMP2012 is not rail-to-rail input. This can be seen in the spec. below:
This spec. shows that the input common mode voltage must sit 1.8 V lower than the supply voltage. For 3.3 V supply then the input common mode…
Other Parts Discussed in Thread: OPA387 , OPA392 , OPA182 , OPA192 TI App Note SLOA059B "DC Parameters: Input Offset Voltage (VOS)" (Richard Palmer and Katherine Li), talks about op-amp input offset voltage but may not contain an answer to the following:…
Hi Renan,
Renan Santos Adriano said: Lets assume that I am taking output from a singular opa387 design at per point 2 and if one of the wheatstone bridge gets unbalanced that is strain guage output changes from 1000ohm to 1015 ohms during strained state…
Other Parts Discussed in Thread: OPA387 , OPA392 , OPA328 , OPA325 , OPA391 , OPA333 , OPA828 , OPA182 , OPA192 , OPA191 , OPA186 , LM7705 Dear all,
In reference to my previous post,
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1188165/impedance…
Part Number: INA333 Other Parts Discussed in Thread: OPA391 , TLV387 , OPA333 , TLV333 , OPA387 , OPA187 Hello
I designed sEMG PCBA with INA333 as first stage of amplifier,first time I used the same SCH as bellow,and the ouput signal is correct.
The secon…
HI Nathan,
We discussed the issue on the OPA376. The datasheet shows the CMRR changes from 90dB @25C to 60dB @150C, at hot temperature, where CMRR is specified above V(-) supply. The datasheet offers no assurances for CMRR for voltage more negative than…
Part Number: LMP2012 Other Parts Discussed in Thread: OPA387 , OPA388 Hello,
I have witnessed that the LMP2012 takes a long time to settle after the input signal switches from one value to another. This settling time and error depend on the amplitude of…