Other Parts Discussed in Thread: OPA4322 , PGA411-Q1 Hello TI,
I have project about EV motor control need you help or suggest suitable TI Design.
Our The 3-phase PMSM spec is power rating 13 KW, 130 N.m, 6000 r/min. Battery Pack Voltage 144VDC.
…
Part Number: TDC1000 Other Parts Discussed in Thread: LMV881 , OPA353 , OPA357 , , OPA322 , OPA4322 , REF2912 Hello. I am testing the Ackerberg-Mossberg bandpass filter and have questions. The filter enters the generation mode and it worries me a lot…
Hi Aj,
what do we see on the scope plots? Is it uncorrelated noise? Or is it the 300kHz signal from the ultra sonic sensor?
The OPAmps: Is it the OPA2322 or OPA4322?
Kai
Hi Jacob,
you violate the common mode input voltage range of LM2901. This chip can only handle input voltages which don't exceed 3.3V-1.5V=1.8V. But the OPA4322 gives out up to 3.2V! You might need a comparator which can input rail to rail.
Kai
Thanks,
OPA4322 can't be used in the LTSpice, so could you help to simulate the circuit for me? What about its performance of envelop tracking with 20KHz sinewave?
BR,
Helen
Leo, OPA4388 will NOT be fast enough to settle to within 16-bit resolution at 1Msps sampling rate. If you use the op amp in an inverting configuration, please take a look at OPA4350 (GBW of 38MHz) while for the non-inverting configuration you should use…
Q1: The UAF42 datasheet specifies under "Filter Performance" that the frequency range, 'fn' is typically from 0 to 100 kHz. Does this mean that if the high-pass filter cutoff frequency is set to 20 kHz, that the pass-band will only extend up to 100 kHz…
Hello,
In that case, I do not know where the oscillations in my signal chain could be coming from. Could I share the schematic with you offline? We are using two TI amps: LMV861 and OPA4322.
Other Parts Discussed in Thread: ADS7263 , OPA4322 Hello,
I am looking to use the ADS7263 in a new design for a 4-quadrant detector (4 photodiode). I already make the sum (A+C) and (B+D) with a OPA4322 and now I have a signal going from 0V to 5V. As…
Other Parts Discussed in Thread: OPA4322 Hello,
An OPA2322AIDR is being using in the attached schematic as a charge amplifier for a piezoelectric receiver array.
With the following parameters:
Input 50ohm-terminated to ground (i.e. no signal…