Part Number: OPA564-Q1 Other Parts Discussed in Thread: OPA564 , Hello team,
When customer tested the OPA564 power supply sequence, measured voltage rose from 0V to 3V, the rise time difference between Vsupply and VDIG was very small, basically the same…
Part Number: OPA564-Q1 Hello team,
About the resistance of θjc and θja, I have read these two reply in the E2E, but I still confused about the θjc and θja
https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum…
Part Number: OPA564-Q1 Other Parts Discussed in Thread: OPA564 ,
I want to find a driver for this DFB laiser, whose parameters are listed as below.
The triangular wave is used as the input to control the Laser, whose frequency is almost 100KHz.
You can…
Hi Jeferson,
Jeferson Pehls said: (1) Do I need to place at the output of OPA564, schottky diodes from GND (or negative power supply) to the output, and from output to the positive supply, so that they act as clampers?
Since you are driving inductive load…
Hi Higa-san,
Please take a look at OPA564-Q1 part, which is automotive grade OPA564. The OPA564-Q1 is revised recently, but it is using the same die design as OPA564.
Daisuke Higa said: 1.Do the above two temperature ranges refer to ambient temperature,…
Part Number: LM675 Other Parts Discussed in Thread: ALM2402F-Q1 , ALM2402-Q1 , ALM2403-Q1 , OPA593 , OPA564 , TINA-TI , OPA564-Q1 Tool/software: Hello.
I'm beginning a project that is a little different for me.
I will show the details I can.
Input:…
Part Number: LM2904-Q1 Other Parts Discussed in Thread: OPA564-Q1 , ALM2403-Q1 , ALM2402F-Q1 Could you pls select a suitable product for me? Thanks!
1) Automotive grade dual-channel operational amplifier
2)Single power supply voltage range 5-24V
3) Common…
Part Number: ALM2403-Q1 Other Parts Discussed in Thread: OPA564-Q1 , ALM2402F-Q1 Hi Team,
My customer Li-Auto is looking for a power op-amp with continuous 800-900mA output for resolver application. Is ALM2403-Q1 able to supply in this application? And…
Hi Yuhua,
育華 詹 said: case 1.
vin = -15V , V+ = 0V ,V- = -24V => This case failed
The OPA564/OPA564-Q1 is able to meet the rising edge requirements from a step voltage of 15V delta (the slew rate is 40 V/usec).
The output voltage range may violate the…