Well Tommy, that LMH6702 is a pretty good choice for an uncommitted current feedback amplifier, an SO-8 package by itself has 0.4nsec delay, so use the SOT23 for sure - another option with internal gain set resistors would be the OPA693. I am guessing…
Other Parts Discussed in Thread: OPA693 , CDCLVC1102 Dear experts,
Customer is looking for solution to replace OPA693(Gain =2, high slew rate : 2500V/us) which is used for 130MHz clock amplifying.
Must Requirement :
Supply : 3.3V, Package thickness : 1.3m…
Part Number: THS4304 Other Parts Discussed in Thread: OPA693 , , THS4302 Dear experts,
Customer is looking for high speed amp to replace OPA693(Gain =2) which is used for 130MHz clock .
Must Requirement :
Supply : 3.3V, Package thickness : 1.3mm under..
…
Hi Neelam,
I would suggest using the OPA692 instead of OPA693 or THS7314 for driving more than two video lines. The linear output current drive for the OPA693 or THS7314 is limited to drive only two video lines, whereas the OPA692 would be ideal for…
Other Parts Discussed in Thread: OPA693 , OPA692 , LMH6704 Hello,
Our customer are searching for tri-level sync signal driver.
The video signal is SMPTE 240M spec.
Could you recommend a good amplifier?
The customer want the amplifier with 6dB fixed gain…
Hello,
Thank you for the answer.
But why not BUF602 or OPA693.
BTW, I`m designing now SPDIF driver circuit for 75 Ohm unbalanced and 110 Ohm balanced with transformers.
I think I can use differential output line drivers for both unbalanced and balanced…
Other Parts Discussed in Thread: THS3201 , OPA693 Hi,
I am looking for a line driver capable of driving a 50ohm doubly terminated coax line with < 3ns rise time and ≥ 300MHz bandwidth. The input is a 0-5V TTL digital input so input impedance must be…
Other Parts Discussed in Thread: OPA693 , OPA360 , THS7314 Hi!
I´m in the need of a composite (PAL) video splitter. Meaning I have one video source in and I want two video sources out. I only have +5v single supply to play with. Would the OPA693 and the…
Other Parts Discussed in Thread: VCA824 , OPA691 , OPA693 , LMH6502 , LMH6503 , LMH6504 , LMH6702 , LMH6703
Hello.
We have a system running at a fixed 175MHz. The VCA824
variable gain amp is used for Amplitude Modulation, the output voltage varies
between…