Part Number: OPA2695 Other Parts Discussed in Thread: OPA695 Hello,
I notice that the dual OPA2695 is covered by a different datasheet to the single OPA695, with the OPA695 looking to be considerably faster in terms of both small signal bandwidth and…
Part Number: OPA695 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hello,
I have schematic as follows: OpAmp_NF_estimation.TSC
Is it correct way to estimate NF of the diff-to-single Op-Amp circuit?
Thank you!
tsa
Hi Rohit, thanks for your quick response.
I managed to recover the password using the visual basic script I found here - it is " AABBBBABABB> ", minus the quote marks and including the > symbol at the end.
Hopefully this is of help to other…
Part Number: OPA695 I need S parameter measurement file of opa695 IF amplifier in order to simulate a GNSS receiver model which contains this amplifier.
Part Number: OPA695 My customer need equivalent (or better) opamp of OPA695 "with offset null pins" in order to control offset externally by means of trim pot.
Some of the important constraints are :
1) Supply should be +/- 5V,
2) Stable at…
Part Number: OPA695 All of the examples in the OPA695 datasheet show the device driving a 100 ohm load. When driving a 50 ohm load, the exanples put a series 50 ohm resistor at the output of the OPA695. We need to send a 40nS linear ramp every 16uS with…
Part Number: OPA847 Other Parts Discussed in Thread: THS3491 , OPA695 , LMH6702 , OPA3695 Dear Sir or Madam,
I would like to use the OPA847 in non-inverting configuration at a gain of 2. Is there a recommended external compensation circuit for this configuration…
Hi Samir,
I agree that the D2S of THS3215 or THS 3217 is quite good. However, the minimum OPS gain of THS3215 or THS 3217 is 1.5. The ideal OPS gain is 2.5 at which most of its electrical characteristics are given. Therefore, the ideal total gain of…
Hello,
the input signal amplitude is 0V~2V, power supply is +/- 3.3V, output amplitude is -2.0V ~ +2.0V, the load is 100 ohm.
how to calculate max current of OP695?
Thank you,
kerb
Hello,
the input signal amplitude is 0V~2V, power supply is +/- 3.3V, output amplitude is -2.0V ~ +2.0V
how to calculate max current of OP695?
Thank you,
kerb