Other Parts Discussed in Thread: ADS1281 , REF5020 , REF5025 , OPA735 , REF5050 , OPA227 , OPA313 , THS4531 , TINA-TI Hi,
I want to design a 8-channels recorder.
I use eight ADS1281 ADCs for synchronized.
The Vref design is from the datasheet of REF50xx which…
Other Parts Discussed in Thread: OPA735 Hi All.
i'm making a inverter amplifier. i configure opam in single supply like application guide "Single-Supply Op Amp Design Techniques" i do it in bread board and simulation in Tina but output alway satturation…
Hi Chris,
About " However, it will not be exactly 5V because the OPA735's output will saturate around 20-50mV from the negative supply rail. "
OPA735 is supplied with +5V and -5V and the output is -2.5V, I think it will not go into saturation…
Hello Paddy,
What is the total supply voltage? It's a little hard to tell. If it's 12V or below, look at the OPA735 for the precision amplifiers, for 36V operation, look at the OPA188 for the precision parts and OPA234 for the more generic amplifiers…
Other Parts Discussed in Thread: OPA735 , LMV641 , LMV841 , OPA2188 looking for OPAMP,Vcc max=12v or more,Offset=less then 60uv,Rail 2 rail,Size=SC70
I found the OPA735 which meet these4 parameters but not in SC70 package.
Other Parts Discussed in Thread: OPA735 , ADS1298 Hello,
I have a problem on the use of REF5025 and it`s application.
One thing I want to be clear is the output noise that looks like triangle wave from the application TI brahs recommanded.
I designed …
Other Parts Discussed in Thread: OPA2209 , OPA735 , OPA727 , OPA277 , OPA704 , DAC8562 , DAC8832 Hi @all,
I'm using the DAC in a high-speed control loop.
Refering to the data-sheep, p.11, I expected a glitch-amplitude of about 20mV.
What I see now, is a…
Part Number: MSP430F5529
Team, I am currently attempting to use an MSP430F5529 to read in an analog value and populate it to an array. I have configured the MSP430 to start a sample conversion off of TimerA0, as shown in the datasheet, but am currently…
Other Parts Discussed in Thread: LM324 , OPA735 , OPA188 , OPA2277 , OPA277 , LT1013 , LM358 Dear Sir,
I am trying to find difference between two voltage sources using op amp. My application goal differentiate the voltage and give to ADC controller and it says…